![]() |
MP3 was removed but fixes were included in MP4 |
--------------
Legal Notices
--------------
©2010 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 102.00.04.03
Date: 08-Mar-2010
This release of Solid Edge has been certified to run on the following:
- Windows XP Professional© operating system (32-bit or 64-bit)
- Windows Vista Business© or Vista Enterprise© operating system (32-bit or 64-bit)
- Windows 7 Professional©, Enterprise©, or Ultimate© operating system (32-bit or 64-bit)
- Internet Explorer 7 or 8 (IE 6.0 minimum)
User Account Control (UAC) -- Due to continued reports of problems with Solid Edge installation and removal, Solid Edge licensing, Insight web parts and other cases writing to text files in the program folder, it is recommended that the UAC be turned off when running on Windows 7 or Vista.
Windows 7: Control Panel -> User Accounts -> Change User Account Control settings ->
Never notify
Vista: Control Panel -> User Accounts and Family Safety -> User Accounts ->
Turn User Account Control Off.
Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
This Maintenance Pack can be installed on top of Versions:
102.00.00.116, 102.00.01.04, 102.00.02.06, 102.00.03.04
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
=====Part/Profile/Sheet Metal=====
PR 1580181: Section view not displaying correctly for valid section lines
PR 1764597: No silhouette available when placing tangential ref plane
PR 1769410: Custom bend formula is ignored for synchronous sheet metal parts
PR 1772130: Axis of revolution command not available when creating a revolution in simplify env.
PR 6250240: License borrowing fails
PR 6268973: Cannot change dimensions after saving
PR 6273326: Cannot place Move/Rotate handle on specific bend axis
PR 6275448: Cannot edit the bend radius after a partial flange is patterned
PR 6283900: Provided files will not save in Windows 7 OS
PR 6296196: Solid Edge aborts trying to redefine flat pattern after deleting tab
PR 6302645: Wrong SEInstallData.dll delivered in x64 folder with 32bit app
PR 6301306: Base contour flange does not use neutral factor
PR 6305404: RMB in background of pathfinder selecting the item to the left
PR 6306428: Failed profile behavior in MP3
=====Assembly=====
PR 1768941: FOA could no longer opened
PR 2139946: Multiple copies of translated components
PR 6050159: Part will not stay up to date
PR 6270986: Simplified Assemblies Causing Relationship Failures
PR 6293937: Assembly aborts when part or relationships are deleted
PR 6298670: Blurry Icons on Japanese command ribbon
PR 6302734: Improved overall performance on Edit, Close & Return, Options dialog, and Show/Hide
PR 1754137: Inter-part Copy command was not available in Design & Drafting
PR 1772048: Bigger part will be excluded when creating a simplified assembly
PR 2139785: Korean Font problem in docking Windows of Explode-Render-Animate mode
=====Draft=====
PR 1760338: Behavior change when moving balloons
PR 1770625: Parts list is not sorting correctly
PR 2140144: Parts list changes spacing in ST2
PR 6267261: Draft Callout Shortcut list not working
PR 6299585: Parts list is missing data on adjustable assemblies
PR 6296029: Block attributes get added to block text values
PR 1756358: Middle mouse button does not work in the Drawing View wizard custom orientation dialog
PR 1772239: Descending sort order not saved to saved settings
===Insight/View & Markup===
PR 6294031: Cannot run CreateInsightFullTextIndexForWSS3 on SSL server
PR 6299605: View & Markup - Part count is incorrect
PR 6307377: Revise fails to correctly set revision letter on released DFT
PR 6227232: Move or Copy Draft of 2 members of FOA converts both to the same member
=====Embedded Client=====
PR 1765035: File Open doesn't show users items when other user items are present
---
End
---
----------------------------------------------------
Maintenance Pack 4 also addresses the following PRs:
----------------------------------------------------
=====Part/Profile/Sheet Metal=====
PR 1746333: Select Manager - Equal Radius does not select all radii that are equal
PR 1756178: Unable to locate keypoints after exiting profile environment - when IPA
PR 1759127: Unable to create a Swept Protrusion as in previous versions
PR 1760836: Switching to Material Outside changes flange length tremendously
PR 1765687: Countersink hole on wrong side of flat pattern
PR 6188740: Cannot edit a cylindrical dimension after a Jog or Bend
PR 6223856: Cannot move a group of faces regardless of the Live Rule settings
PR 6225736: Moving a face until it fails removes color on faces
PR 6231047: Unable to move face of a revolved protrusion in this converted synchronous part
PR 6248295: Color overrides are lost after moving a thickness face on converted or imported part
PR 6258514: Options button goes away during Section view command
PR 6266350: QuickPick on 2D constraints
PR 6268499: Failure moving a flange in one direction, succeeds on another
PR 6268537: Close Corner fails when adjacent face has a through-all hole
PR 6271426: Cannot rotate a face on a Contour Flange a 2nd time
PR 6271535: Temperature loads are not being calculated correctly for thermal expansion
PR 6271683: Cannot edit the model after a cutout interacts with bend/close corner
PR 6272188: Bend regions do not merge correctly when closing a cross-bend cutout
PR 6272409: Operation Unsuccessful moving face on Contour Flange
PR 6272878: Thickness faces do not merge when creating Contour Flange
PR 6273983: Need to prevent the creation of a Contour Flange on a circular tab
PR 6274434: Unable to add procedural feature to circular flange pattern
PR 6274536: Regression editing a Contour Flange with Concave corner
PR 6276005: Moving a thickness face on this part causes cutout to change size
PR 6279114: Contour Flange does not go to tangents of bend if profile has curve outside the face
PR 6281152: Changing depth of tapered hole during placement is not being handled properly
PR 1766139: Simulation Express cannot analyze small parts; meshing fails
PR 6244242: Unable to change direction of dimension edit on chained dimension
PR 6251970: After rotating face you cannot move any faces on model
PR 6259374: Simulation is using the old Femap mesher
PR 6263297: Switch to flat pattern in synchronous sheet metal causes views to go out-of-date
PR 6269384: Live Rules - inconsistent behavior depending on when selected
PR 6269974: Crashlogs for Windows 7 list the OS as Vista
PR 6272097: After failure editing dimension in glass sheet mode you get a "break" Failure
PR 6272411: File has a pattern that you cannot delete
PR 6276824: Cannot delete a Contour Flange with Closed Corner or small Circle cutout
PR 6277695: Cannot create a 360 degree internal hem in synchronous sheet metal
PR 6283174: Hang when editing a dimension value and pressing Enter and another key simultaneously
PR 1754499: Certain constraint conditions are not reporting errors
PR 1765060: Problem with Neutral Factor
PR 1766833: Custom bend formula does not work correctly on STEP imported PSM
PR 2086784: Assembly section view not cutting the body
PR 6114037: Unable to rotate part faces
PR 6258865: Undo is being disabled when editing the profile of non-base features
PR 6260823: Display performance during dynamic rotate is bad
PR 6285483: Fixed distance is not maintained when editing an Angular dimension
PR 6287803: Problem with weldment running out of memory after edit
PR 6288372: Select command is not available in Customize QAT
PR 6288463: Dimension group is collapsed in profile environment at low resolution
PR 1753048: Problem editing threads
PR 1767777: Impossible to modify material thickness of the provided sheet metal model
PR 6267593: Thread lines in draft are lost after a face move
PR 6296531: Incorrect 'Mapped Meshing Option' is used
=====Assembly=====
PR 1702605: Parts have wrong position after replace part, but system gives no error
PR 1762724: The relationship icon is not updating correctly when switching to FlashFit
PR 1762903: Unsuppress of a pattern was not recreating the slave parts
PR 2112786: Motor direction is not reversing correctly in this model
PR 6237593: Undo is not updating moved faces in a translated assembly
PR 6242099: Failed PMI dimension appears to dramatically affect performance in this assembly
PR 6248060: Relationships failing when replacing a subassembly using same base part
PR 6274831: Menus defined in Environment Motion via Add-In prevent upgrade of add-in
PR 1757437: Drawing Views are permanently out of date in the provided file
PR 2134132: File load failure; list is copied incompletely
PR 6097501: Groove welds/fillet welds fail when parts are inactive
PR 6275140: Temp license for simulation gives X number of day’s left message regardless of duration
PR 6281888: Getting simulation license expired message
PR 1763130: Adjustable part pattern does not behave the same as it did in V18
PR 6262448: Get a display error message when transferring into an FOA file
PR 6283906: Problems with assembly features failing on file open
PR 2134733: Parts list is incorrect for an FOA member
=====Draft=====
PR 1751242: Drawing view could not be updated view after changing source from a weldment to assembly weldment
PR 1752368: Improved performance issues with drawing view update
PR 6275441: User data is lost when parts list is pasted
PR 6281484: Parts list is missing when opened in ST2
PR 6285477: Solid Edge crashed when entering text into combo box
PR 1715016: Dimension values will not move, when DV is moved
PR 6283924: Parts list failed after it was copied and changed to another model via edit links
PR 1754125: Projection line breaks do not print
PR 1760828: Difficult to locate broken out section profiles and problems with fitting drawing views
PR 2130190: Added new automation for section view boundaries
PR 6276308: Solid Edge is crashing during Save after placing a connector, then deleting
PR 1684715: Showing hidden lines did not set drawing view out-of-date in some cases
===Mold Tooling===
PR 1751932: Product aborts when opening, saving and closing a Mold Tooling subassembly
===API===
PR 6266016: SEInstallData unable to return information
PR 1767753: Contour flange is failing when bend table is called
===Insight/View & Markup===
PR 6274801: Revise fails when “Who can view membership of the group” is set to members only
PR 6262986: Cannot save PCF in Revision Manager, managed or unmanaged
PR 1762264: A mixture of A4 Portrait and A4 Landscape stretches view in View & Markup
PR 1766363: Wrong value for Revision Number is generated for implicit revised draft files
PR 6284707: Cannot get full text index created
PR 6287309: Assembly cannot be moved from Available to Released - Cannot Change Status
PR 1767035: Assembly cannot be moved from Available to Obsolete - Cannot Change Status
PR 6293898: Solid Edge fails to open file after selecting from Insight Dash Board
PR 1766879: Revise will set an incorrect value for SharePoint column SERevisedFrom
PR 6281407: Opening Revision Manager causes an Insight error
=====Embedded Client=====
PR 6279117: Uploading a file that is stored in Teamcenter allows the user to change the Item type
PR 6279218: Solid Edge crashing after mapping date custom property to a text attribute
PR 2135433: Certain user accounts can't create/save a draft file
PR 6272925: Solid Edge Structure Editor crashes when selecting List of Values
PR 1756631: Preference “SEEC_BOM_Synchronize” does not work with assemblies
PR 6298313: The data prep analyze tool does not read the csv files correctly for foreign locales
---
End
---