Solid Edge ST7 SDK
Solid Edge ST2 MP6 - Readme

--------------
Legal Notices
--------------
©2010 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        102.00.06.04
Date:           13-May-2010

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
102.00.00.116, 102.00.01.04, 102.00.02.06, 102.00.03.04. 102.00.04.03, 102.00.05.04


This release of Solid Edge has been certified to run on the following:

   - Windows XP Professional© operating system (32-bit or 64-bit)
   - Windows Vista Business© or Vista Enterprise© operating system (32-bit or 64-bit)
   - Windows 7 Professional©, Enterprise©, or Ultimate© operating system (32-bit or 64-bit)
   - Internet Explorer 7 or 8 (IE 6.0 minimum)


User Account Control (UAC) -- Due to continued reports of problems with Solid Edge installation and removal, Solid Edge licensing, Insight web parts and other cases writing to text files in the program folder, it is recommended that the UAC be turned off when running on Windows 7 or Vista.  

        Windows 7: Control Panel -> User Accounts -> Change User Account Control settings ->
                   Never notify

        Vista:  Control Panel -> User Accounts and Family Safety -> User Accounts ->
                Turn User Account Control Off.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===
PR 2143986:  Problem with the use of the API "UseGlobalBendRadius Property" in VB code
PR 1780296:  Abort after GoTo on moved feature within a sheet metal file
PR 6325660: Cannot access Parts List thru Sheet:DrawingObjects automation
PR 6333911: Exposed AttributeSets API on Block

=====Assembly=====
PR 1747958: Model is not recognized as symmetric in assembly mirror function
PR 1751920: Assembly features do not work correct, when parts are inactive
PR 1755903: Assembly features do not work correct, when parts are inactive
PR 1765375: Preview Angle Control does not update
PR 1778358: Crash when editing a feature that does not modifying any parts
PR 6292316: Crash on close or won't open the file again after updating views
PR 6327304: Rack & pinion not working in Engineering Reference
PR 1760454: Importing/Opening a Catia assembly results in an empty file
PR 6342529: Unable to successfully update Standard Parts framework
PR 1732510: Export ASM to SAT results in an empty file

=====Draft=====
PR 1779564: Parts list is not displaying on open under certain conditions with a non-English locale
PR 1781702: Model out-of-date condition was shown incorrectly when updating a part copy
PR 6291000: Strange display behavior in draft on the drawing sheets
PR 6331849: Aborting while deselecting annotations
PR 1783893: DXF3D translation SAT generation fails
PR 1778320: Property text displaying errors instead of blank for some physical properties
PR 2144635: Connectors are moving to the origin of the file on open

===Insight/View & Markup===
PR 6334670: Saving a STEP file to SharePoint leaves the file checked out and won't allow
PR 6331332: Rev Mgr crashes when copying FOP master when it is open in Solid Edge
PR 6328368: Where Used is not working in Revision Manager after upgrade to WSS 3.0
PR 6339445: VB6 Program to retrieve Solid Edge Docs by File Properties doesn’t work with ST2

=====Part/Profile/Sheet Metal=====
PR 1781604: Sheet Metal file aborts during a Flat Pattern creation
PR 1781678: Flange length is wrong when using a keypoint + option measurement outside
PR 6316315: Suppressing a pattern occurrence does not work correctly
PR 6322150: Maintain Relationships gets turned off in Profile if changed in Sketch
PR 6331560: Unable to edit sheet metal model at current state
PR 6334956: Display performance is bad in the provided case
PR 6323762: Hole becomes sick when editing a dimension on an unrelated hole
PR 2143188: Incorrect indication of an under constrained profile in Pathfinder
PR 6339460: Unable to save a part file after a network drop and reconnection
PR 1784612: Unable to edit the diameter of a cylinder that contains a chamfer
PR 6344677: Edge mesh control is not applied properly
PR 6343510: The widescreen ribbon is not display on monitors that are 1600 pixels wide

===== Solid Edge Embedded Client=====
PR 1779190: Saving and uploading an assembly is incrementing the quantities in the BVR
PR 6314396: Doing SaveAs (or Revise) selected with FOA member load crashes Structure Editor
PR 6314693: SaveAs does not load associated draft file via interpart links
PR 6337991: Revision of part copy cannot be replaced in Structure Editor


---
End
---