--------------
Legal Notices
--------------
©2010 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 102.00.07.04
Date: 28-Jun-2010
Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
This Maintenance Pack can be installed on top of Versions:
102.00.00.116, 102.00.01.04, 102.00.02.06, 102.00.03.04. 102.00.04.03, 102.00.05.04,
or 102.00.06.04.
This release of Solid Edge has been certified to run on the following:
- Windows XP Professional© operating system (32-bit or 64-bit)
- Windows Vista Business© or Vista Enterprise© operating system (32-bit or 64-bit)
- Windows 7 Professional©, Enterprise©, or Ultimate© operating system (32-bit or 64-bit)
- Internet Explorer 7 or 8 (IE 6.0 minimum)
User Account Control (UAC) -- Due to continued reports of problems with Solid Edge installation and removal, Solid Edge licensing, Insight web parts and other cases writing to text files in the program folder, it is recommended that the UAC be turned off when running on Windows 7 or Vista.
Windows 7: Control Panel -> User Accounts -> Change User Account Control settings ->
Never notify
Vista: Control Panel -> User Accounts and Family Safety -> User Accounts ->
Turn User Account Control Off.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
===API===
PR 1780429: VB.NET Program cannot save a simple assembly file
PR 1783822: PartsList.Add method is not using predefined origin
PR 6342066: API 'SelectSet.Add' is not working with Parts list object
=====Assembly=====
PR 1785407: Performance delay when using Title in the "Document name formula"
PR 6338066/6339460: Save fails after network disconnect then reconnect
PR 1719100: Unconstrained part in an assembly does not get positioned relative to coordinate system
PR 6313967: Solid Edge aborts when deleting files from the File Open dialog
PR 6324336: Wireframe mode is using part edge color
PR 6357189: Crash in axis dimensions resolved based on auto-capture crashlog
PR 1790105: Active parts are not shown in the provided assembly
PR 1790461: Part is no longer displayed after editing an assembly hole feature
PR 6260509: Improved locate sort order for in-place active subassembly cases
PR 6343399: Appearance events are not working properly in Virtual Studio
PR 1790001: Creating a revolved assembly feature cutout, results in broken silhouette edge links
PR 1791570: Assembly features are in a warned state when opening with parts inactive
=====Draft=====
PR 1780236: Legacy hole table does not use drawing scale when updated
PR 6311605: Parts list copy to clipboard is omitting the last character return
PR 1785794: Provided Draft file does not open
PR 2146859: Parts list title is changing
PR 6355444: Detail Views Go Out of Date when detail envelope is moved
PR 1779926: Cannot copy and paste balloons of part list
PR 1787190: Copy/Paste in draft works only once from MP4 to MP5
PR 6311777: FOP table variables removed when opened in ST2
PR 1694036: The Save Copy As command is not available in Part if opened by double clicking a Drawing view
PR 1760632: Cropped boundary is not displayed correctly on revolved section view
PR 1789683: Parts list is missing when an old draft file is opened
PR 6308835: Cannot show cropping edges on a detail view derived from a revolved section
PR 6361317: Detail view on revolved section view always shows as out-of-date
PR 6247587: Draft Callout.txt is not honoring custom reports location.
Note: The fix for 6247587 will result in properly searching for the DraftCallout.txt
saved settings file in the user-defined Reports folder. If you set a user-defined reports
folder and use callout saved settings, then you need to manually move or copy your existing
DraftCallout.txt from the …\template\reports folder to your user-defined reports folder.
===Insight/View & Markup===
PR 6315177: Problem with Full Text Search in Insight ST2 MP2 when modifying DFTs
PR 6342891: Unable to copy files with linked Excel spreadsheets
PR 1790756: Undo Check out of a modified file saved (Cache) does not delete the changes
PR 6362669: Editing properties in Search Property Manager on open file results in lost work
=====Part/Profile/Sheet Metal=====
PR 1780116: Cannot move holes in a part that has been converted from traditional to synchronous
PR 6278206: Crash in Variable Table command resolved based on auto-capture crashlog
PR 6340132: Advanced Live Rules Tree View will not deselect faces
PR 1784612: Unable to edit the diameter of a cylinder that contains a chamfer
PR 6282481: Feature from feature library is not placed correctly
PR 6360890: Unable to open an NX 7.5 document in ST3
PR 1753614: A chamfer with equal setbacks at non perpendicular faces are not maintained
PR 6360783: Can't change the font size of PMI Annotations in converted Synchronous file
===== Solid Edge Embedded Client=====
PR 1785898: Importing large amounts of data to TCX fails due to the space separator in Swedish locale
PR 1787630: AddToTeamcenter does not create a precise BOM if an item exists
PR 1783479: PDF files created after Save All with multiple draft datasets open are wrong
PR 1788838: AddToTeamcenter fails to import .xls file
PR 6356301: Duplicate entries created in BVR after IPA
---
End
---