Solid Edge ST7 SDK
Solid Edge ST3 MP1 - Readme

--------------
Legal Notices
--------------
©2010 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        103.00.01.05
Date:           24-Nov-2010


Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
103.00.00.114


This release of Solid Edge has been certified to run on the following:

- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit)
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit)
- Internet Explorer 8 (IE 6.0 meets minimum requirements)
 
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===

PR 1810104: SEReader.dll cannot be unregistered
PR 6433759: Crash occurs in ribbon customization when calling EndCustomization
PR 6426380: Not getting Colors in SEPartReader, SEReader
PR 1816843: FamilyMember.Apply API method fails when part document is opened as invisible
PR 6426239: Added a new CheckBOMStructure API

===Assembly===

PR 1787825: Fixed an abort when editing failed assembly relationships
PR 1796377: Cannot open a file with Russian characters in the file name
PR 1807952: The axis for a revolved cutout is not updated when the linked sketch is modified
PR 6159008: Copied Sketches have broken Links in assembly that don't update
PR 6347918: Center line is not being displayed for pipes with a penetration cut
PR 6355912: Cannot create automatic connectors in Simulation
PR 6400068: Assembly feature cutout results in a warning
PR 6410877: Mesh and Results are marked OOD when hiding the connector mesh
PR 6410972: Pathfinder display does not update weld beads properly
PR 6411209: Look at Face not working when selecting an item from the assembly Pathfinder
PR 6412454: No redo log created after deleting a hole
PR 6412858: Edit of an included edge does not work
PR 6413477: Fastener Systems hangs when changing to Gost Standard
PR 6414088: Frame members with assembly features cannot be differentiated using mass uniqueness criteria
PR 6414695: Crash while in the Assembly explode environment
PR 6414712: Part with Inter part links is not updating when master file is edited
PR 6414800: Unable to delete relationships selected in the Pathfinder with the Delete key
PR 6414955: Moving a part with an assembly feature can cause assembly features not to update
PR 6415436: after adding a sub-assembly to a Top Level config, the sub doesn't show
PR 6415933: Solid Edge switches from pathfinder to Engineering Ref tab when you get out of profile
PR 6417247: Configuration Manager is not clearing the "New components" list when unchecked and saved
PR 6417768: Unable to select simplified assemblies
PR 6417909: Docking panes pop out when you switch from Simplify to Design
PR 6417945: Location of the Quickbar / pathfinder isn't correct
PR 6419986: Clicking in Pathfinder will copy component into Assembly
PR 6420539: Custom properties are not showing in the reports
PR 6423879: Part Coordinate System is not visible when turned on from Assembly
PR 6426469: Drop list in Interpart Mgr dialog sorts alphabetically
PR 1814714: Assembly-Driven Part Features are failing after suppress/unsuppress
PR 6425915: Edit dimension dialog not shown to edit spread distance
PR 6427101: Accidental drag copy of parts from ASM pathfinder
PR 1814708: Some commands are not available through keyboard customization
PR 6317812: Fixed a performance problem in FlashFit
PR 1747708: Representation of an alternate assembly is wrong
PR 1814953: Sync Assembly section disappears
PR 6434952: Get different number of relationships if use Update or not
PR 6436335: Solid Edge aborts when specifying a LinkMgmt.txt file
PR 6437668: Drag Component does not move sub-assemblies
PR 6425711: Unable to choose a specific reference position in pattern command
PR 6437611: Modified triad display priority to be above select set

===Draft===

PR 1805793: Parts list does not sort correctly when total length is selected
PR 1805938: Parts list is positioned wrong
PR 1808576: Drawing Sheet contents disappeared after fit
PR 1810153: Counterdrill hole settings are not saved
PR 2154348: A drawing view update consumed a lot of memory and caused Solid Edge to close
PR 6228359: Border line type rendering is not accurate, dashes merge into solid
PR 6404199: Property text is not using escape char when converting old files
PR 6406522: Translation error appears on opening DXF files and fails to import the DXF files
PR 6407712: Balloon contains wrong item number
PR 6408584: Drawn in view dimensions are incorrectly marked as detached
PR 6409957: Cropped edges no longer display when views are shaded and updated
PR 6410140: Spacing wrong when using dual units in a formatted callout
PR 6411077: Parts list copy to clipboard format is different for reverse order of entries
PR 6411847: Dimensions change or detach in a section view
PR 6412902: PMI balloons are not updating when item number options changed
PR 6412998: section view is empty after update
PR 6413947: Geometric rebinding is not working properly in some cases
PR 6414873: Delete key doesn't work for surface texture symbol w/o leader
PR 6416721: Weldment occurrence item number changes when expanding weldment
PR 6417349: Move elements to layer button always being enabled
PR 6419362: Incorrect mass in exploded parts list when quantity overrides exist on sub-assembly
PR 6424154: Callout value is not shown when using "Variables from active document option"
PR 1818435: User-defined data is removed from parts list when updated
PR 2157944: Cut length is blank if value is approximate
PR 6430676: Some textboxes are being stretched horizontally
PR 1798788: Dimensions detach after copy/paste/update of revolved section view
PR 1810175: Crash during Replace Block
PR 6422866: copy/paste of drawing views
PR 6437624: user cannot delete curves after fence selecting them
PR 6438159: section view is going away after update.
PR 6440087: Copy/paste doesn't work

===Insight/View & Markup===

PR 6386605: Degree symbol in Document Number gets converted to a long string of garbage
PR 6407475: Error message received when revising
PR 6408201: Cannot successfully add to library from Win764 using 64bit Solid Edge
PR 6413940: Property Manager is displaying values in wrong fields
PR 6414056: Create Insight Full Text Index incorrectly adds -t 7608 switch to SQL Server
PR 6428697: Get and error when installing Insight Server for SharePoint 2010
PR 6429274: Can't run the Create FTS catalog
PR 2157301: Unable to run Insight Server Assistant in ST3
PR 6433176: Insight server - Spanish - Properties are not Synchronized on Save and Upload
PR 6433729: Opening assembly brings down the wrong parts associated with sub assemblies

===Part/Profile/Sheet Metal===

PR 1808975: Cannot include elements in a sketch
PR 1812105: 'Move to Synchronous' fails for the whole feature tree
PR 1812196: When the provided sheet metal file is recalculated, flat pattern fails
PR 1812493: Feature options cannot be applied to the model
PR 1813627: Move features using a dimension has changed from ST2 to ST3
PR 6255537: Changing Datum Reference terminator to line causes the DR to move with rotate
PR 6258876: dimension does not behave as expected in sync sheet metal file
PR 6260768: Regions are not being updated correctly
PR 6397949: Sheet Metal - Cutout does not work
PR 6409937: File Save causes an abort with specific files
PR 6411029: Can't locate the midpoint of a blend
PR 6411128: Eng Ref pane popping out when switch to Ordered mode
PR 6413862: File Save causes an abort
PR 6413990: Sync flat pattern does not go OOD after changing to custom bend equation
PR 6414233: Auto MR is creating sick relationships and tangent relationships
PR 6414538: Convert to Sync of this part has gone from 6sec to almost 5min
PR 6416160: Can't change material thickness when file contains partial flange
PR 6416247: cannot get to options dialog in Draft Face Analysis using "horizontal toolbar form"
PR 6416940: While in Simplify if you select Sync feature you can move it
PR 6416949: RMB in the Background after selecting Faces in User Defined Set causes crash
PR 6417958: Cannot place a Smart dimension to and edge if a VV exists
PR 6418759: Enable Find/Save relationships when interpart faces are used.
PR 6420001: getting a stale display in part after undo and sharpen
PR 6420295: FOP does not seem to generate the geometry for all members
PR 6420619: Cannot change the length of a threaded cylinder with Dimension
PR 6420730: Pathfinder Links shows wrong information when a file has been removed from asm
PR 6421068: Crash trying to open specific pwd file
PR 6423669: Thinwall command in ST3 Sync does not have add option
PR 6426406: Crash trying to run “Transform to Sheet metal”
PR 6335737:  Dimension takes 29 seconds to configure in one direction
PR 6360199: No concentric Live Rule found on test case
PR 6400093: Feature relationships are lost from version 20 to ST2
PR 6414458: part disappearing from pathfinder when moving a face in asm
PR 6421078: Attaching PMI (from create 3D) is attaching to rounds on the edges of the part
PR 6426399: Faces on the curved edges not being part of the body when Save as Flat is used
PR 6428595: Zero dimensions do not display on 32-bit Solid Edge
PR 6222922: Copy-Paste-Attach of Flange and Drawn cutout problem.
PR 6427604: Equal Radius for cones is finding unequal radii cones
PR 6418100: 3D driving dimension moves from original location during edit
PR 6435902: Moving origin of move handle over faces is slow, jerky
PR 6437377: Cannot relate to a feature origin.

===Solid Edge Embedded Client===

PR 1795522: SEEC Wrong types of Item object created for SE datasets
PR 1807349: Empty JT-file in TcX-Viewer
PR 6395864: Structure Editor takes too long to open assembly
PR 6408271: SEEC Integrate 3rd Party Drop
PR 6414597: In the specific workflow, when you In-Place-Edit a component it will be READONLY
PR 6416470: "From linked 3D" does not copy the properties from linked file to the draft
PR 6417113: Desc: Value not shown for property Author when item type is changed


---
End
---