Solid Edge ST7 SDK
Solid Edge ST3 MP10 - Readme

--------------
Legal Notices
--------------
©2012 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        103.00.10.04
Date:           20-Dec-2011

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
103.00.00.114, 103.00.01.05, 103.00.02.04, 103.00.03.04, 103.00.04.05,
103.00.05.03, 103.00.06.05, 103.00.07.05, 103.00.08.06, or 103.00.09.05.

This release of Solid Edge has been certified to run on the following:

- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit)
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit)
- Internet Explorer 8 (IE 6.0 meets minimum requirements)
 
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, unbundle the zip file and
then dbl click on exe to install the Maintenance Pack.

Windows 7 Installation tips: In addition to turning off UAC, right click on the exe
and select "run as administrator" to complete the installation.

Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing
Solid Edge somewhere other than the default “Program Files” folder. Install in a location
like c:\SolidEdge\ that the user has full permission to write to.


-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===

PR 1866474: Added API to get FillStyles from assembly document
PR 6634888: SolidEdgeFramework.ISEECEvents.SEEC_BeforeCPDDisplay fails for revise

===Assembly===

PR 1870427: Cannot associatively include in the provided assembly file
PR 1870566: Pathfinder displays assembly structure incorrectly
PR 2169467: Issue with frames and alternate assembly, no frame is created
PR 2175535: Frame error after deleting frame from an FOA
PR 6590407: seiges.exe executable crashes
PR 6405597: File cannot be saved if disconnected/reconnected to network

===Draft===

PR 1856141: Tables are not exported to DWG if Enable Layer and Attribute Mapping enabled
PR 6594495: not able to extract properties thru callout on some blocks
PR 6605978: Fixed a crash on file close submitted via crashlog
PR 6617549: Fixed a random crash submitted via crashlog
PR 6622040: Simple drawings take a long time to open or save
PR 2174964: Unnecessary leader (Arrow) is displayed in this draft file

===Insight/View & Markup===

PR 1869597: Print Drawings tool isn't downloading the drawings to cache

===Part/Profile/Sheet Metal===

PR 1862813: Inconsistent unit for moments of inertia
PR 1863908: etch not exported to DXF
PR 1866347: save as flat with etch of single line text has unstable behavior
PR 1857104: Wrong threaded Holes (from prev. SE-Version) not getting right
PR 1866914: FOP members do not update correctly. Every dimension which was set as "Distance”
PR 6612183: abort using the include profile command between parts -64-bit only
PR 1875302: FOP table dimensions in draft are incorrect
PR 1867194: No Copy of Synch Feature
PR 1874969: Family of Parts drawing shows wrong dimensions

===Solid Edge Embedded Client===

PR 6586193: Crashing after user gets logged in but performs no operations

---
End
---s