Solid Edge ST7 SDK
Solid Edge ST3 MP12 - Readme

--------------
Legal Notices
--------------
©2012 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        103.00.12.03
Date:           25-May-2012

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
103.00.00.114, 103.00.01.05, 103.00.02.04, 103.00.03.04, 103.00.04.05,
103.00.05.03, 103.00.06.05, 103.00.07.05, 103.00.08.06, 103.00.09.05,
103.00.10.04, or 103.00.11.04.

This release of Solid Edge has been certified to run on the following:

- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit)
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit)
- Internet Explorer 8 (IE 6.0 meets minimum requirements)
 
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, unbundle the zip file and
then dbl click on exe to install the Maintenance Pack.

Windows 7 Installation tips: In addition to turning off UAC, right click on the exe
and select "run as administrator" to complete the installation.

Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing
Solid Edge somewhere other than the default “Program Files” folder. Install in a location
like c:\SolidEdge\ that the user has full permission to write to.


-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===

PR 1882889: Message "Network error has been detected..." appears after calling GetReadOnly
PR 1864732: "SaveAsToTeamCenter" takes a long time

===Assembly===

PR 1854958: Parts are not displaying correctly when switching between alternate assembly members
PR 1871143: Edit subassembly in place collapses assembly PathFinder, regression from V20
PR 1878853: New part added to pattern with suppressed occurrences cannot be suppressed
PR 6612747: Abort after using Animation Editor
PR 2186316: Auto-restore is not working when using backups

===Draft===

PR 6596387: When saving this draft file, Feature Control Frame moves
PR 2192760: V20 draft file aborts when opened
PR 1849055: Solid Edge Draft Crash

===Insight/View & Markup===
PR 1849487: Poor Search performance caused by sub-optimal SQL query statements
PR 1896255: Optimized SQL query code
PR 6571023: Search aborts IE or can hang Solid Edge if stopped

===Part/Profile/Sheet Metal===

PR 6645336: Sold Edge crashes on app close after going into FOP and AA table
PR 1872273: Problem during Save As in Multisite environment

===Solid Edge Embedded Client===

PR 1862616: Extended Standard Parts have an inconsistent ItemID
PR 6561690: File open will not display folder content


---
End
---