--------------
Legal Notices
--------------
©2011 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 103.00.02.04
Date: 12-Jan-2011
Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
This Maintenance Pack can be installed on top of Versions:
103.00.00.114, or 103.00.01.05.
This release of Solid Edge has been certified to run on the following:
- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit)
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit)
- Internet Explorer 8 (IE 6.0 meets minimum requirements)
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
===API===
PR 2153824: Japanese text input in a custom property is garbled
PR 1823741: Wrong behavior of the instruction "objapp,runmacro" in SE ST3
===Assembly===
PR 6454482: Moving multiple parts with Drag Component in the ERA environment causes an abort
PR 1818779: Assembly aborts creating a Groove Weld
PR 2157042: Assembly report command could not find template file because it is Unicode issue
PR 6436398: Material Table is not updating from Solid Edge Admin
PR 6437662: When the provided JT file is opened in Solid Edge the product aborts
PR 6438181: Edge connection is not working in modal analysis
PR 6409833: Piping does not update when adding a gradient angle to path
PR 6427505: 'Use thickness from sheet metal' is grayed out
===Draft===
PR 2155723: Creating new configuration file causes Solid Edge to stop responding
PR 1807028: Translate Part layer names as AutoCAD layer names results in blank file names
PR 1796250: Callout break-line cannot be shortened, when text is vertical
PR 1821014: Saving drafts with shaded views and PDF options takes too long
PR 6450417: Limit dimension - tolerance values are not shown
PR 1819033: Property Text inside a block has a large space between characters
PR 1821130: Tables in a block is causing performance problems
PR 1823434: Hole table values are incorrect
PR 1823724: Textboxes are re-sized on open
PR 1823793: Cannot turn leader on for stacked balloon
PR 2160958: Points are not visible unless the weight is greater than .35
PR 6415363: After using paste special with link option, the excel sheets disappear
PR 6398580: Crash in Push Down command
PR 6431871: Save as PDF has scale problems
PR 6438636: Sheet numbers are not updating
PR 6452718: Several files are crashing when doing a Move to Sync on the last feature
PR 6452738: DraftWeld.txt file is not being used
PR 6453804: Incorrect hatch values when exported to AutoCAD
PR 6460170: Draft file containing empty FOP table crashes on open
PR 1816275: Creating a new file selects the wrong template
===Insight/View & Markup===
PR 1799833: Exception in Models object when running in Insight environment
PR 6441130: Title is not being added to SharePoint during initial save to doc lib
PR 6335967: Rename is not updating Interpart links in Insight
PR 6416289: Open Checked-Out Document from Hyperlink is not Read Only
PR 6448951: Save As does not check in the new file
===Part/Profile/Sheet Metal===
PR 6451312: Display Anomalies: Display of value dialog boxes remain displayed on screen
PR 1814981: Property Manager will not change material on inactive parts
PR 1820819: Model failing after adding a round to a Pattern
PR 6395297: Long configure time to move a chain of sheet metal thickness faces
PR 6434445: Mirror1 feature is not up to date
PR 1821322: In Solid Edge ST3 is error in translation file create in ST2 to .SAT
PR 6449594: Sync Pattern does not update when parent feature draft angle is changed
PR 1821950: Neutral Factor and material thickness cannot be changed with this workflow
PR 1823539: Cannot move or copy a cutout with a break corner
PR 6417621: Curve by table does not work with Office Pro 2010 (32 bit)
PR 6449242: Paste sketch is leaving behind objects used for dynamics
PR 6453756: Holes do not stay concentric
PR 6455614: direction 2 controls being disabled when placing a crown on a symmetric extrude
===Solid Edge Embedded Client===
PR 2155011: Smart Codes do not recognize name rule for custom Item type
PR 6424076: Creates BOMLine for Zero Length Pipe Segment
PR 6427105: User can checkout a file on two computers at the same time
PR 6434610: Edits to variables are taking entirely too much time compared to unmanaged edits
PR 6417804: Dry run not detecting duplicate Item ID or existing dataset in Item Rev
PR 6401679: Save As Draft puts the part & JT data under the old item revision.
PR 6428548: Standalone SESE display generic icon in open dialog, instead of SE icons (F)
PR 6456355: SEEC Search w/ TCX 5.3 aborts
PR 6454638: CPD does not dispay the fixed value and does not have a assign on a field
---
End
---