Solid Edge ST7 SDK
Solid Edge ST3 MP5 - Readme

--------------
Legal Notices
--------------
©2011 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        103.00.05.03
Date:           09-May-2011

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
103.00.00.114, 103.00.01.05, 103.00.02.04, 103.00.03.04, or 103.00.04.05.


This release of Solid Edge has been certified to run on the following:

- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit)
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit)
- Internet Explorer 8 (IE 6.0 meets minimum requirements)
 
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===

PR 1839182: Cannot add a reference object created from top doc to active select set -when IP
PR 6522541: Needs to add Edit, Activate and Inactivate to QAT

===Assembly===

PR 1842534: seSTEP.exe doesn't work anymore
PR 1601738: Family of Assembly member pattern occurrences not excluding correctly
PR 1825923: Colors for stress seems to be incorrect, compared to the values for examination
PR 2164529: Model is not show on Solid Edge ST3 x64
PR 2167384: "Solid Edge" ends when closing this file
PR 6441781: File names in binder are displayed as Chinese or Japanese
PR 1829742: Some surfaces in an assembly are hidden after editing a part
PR 1831430: Simply Motion data is not saved in ST3 64 bit
PR 1842199: Fixed a crash based on crashlog-files (JDisplaycacheWindow)
PR 6522440: Replace part fails to replace when the shared directory is on a mapped drive
PR 6407536: Problem with drafts of assembly weldments with features
PR 6522087: Crash when switching from level based item numbers to another type

===Draft===

PR 1827357: Problem with item number page after assigning "use assembly item numbers"
PR 1829142: Total length value jis blank when approximate lengths are present
PR 1841235: performance when switching to and from 2d Model sheet
PR 1842416: Incorrect mass for exploded parts list
PR 2166838: abort during drawing view update due to unexpected data
PR 6484441: Reference dimensions have extra brackets when exported
PR 6516798: Cannot clear underscores in FOP table
PR 1842000: There is a gap between leader and break line of a callout in certain positions.
PR 1843885: Fixed an abort when using DV query for tube components
PR 1844105: Dragging a block will crash Solid Edge
PR 1844444: Fixed a performance problem in inactive/activate drawing views workflow
PR 6521306: Centerlines highlighting, but not connecting to Centermarks
PR 6521622: Cannot turn on leaders for detached balloons in ST2 drawing
PR 6524478: Callout justification changes
PR 1823729: Hidden groups and layers exported as visible to dwg

===Insight/View & Markup===

PR 1841343: Insight Property Mapping wrong for renamed SharePoint columns
PR 1844782: Insight wildcard search doesn't return a result
PR 1844895: Crash "Create in Place" in Insight Managed Environment
PR 1845737: Sporadic problem during file open. Returning error "Cannot find the file ..."
PR 1845787: Insight attempts access of files on old server when opened by last user saved
PR 6511499: Insight Connect is crashing while attempting a Where Used
PR 6525580: Capture details in an Insight log and display simple and meaningful message

===Part/Profile/Sheet Metal===

PR 1824515: Unable to checkout ST3 license with VPN connection
PR 1836375: After attempting to load a BAS file containing formula SE crashes
PR 1841558: FOP population taking an excessive amount of time
PR 6456015: Coplanar Axis Live Rule not honored after Move to Sync
PR 6488086: Crash trying to edit a dimension in Variable table
PR 6515922: Lofted Flange has flat pattern but fails to produce Save As Flat DXF file
PR 1843052: Abort when creating a cutout in a sync part
PR 1844652: an abort while trying to add a mounting boss feature
PR 6426519: Fixed a performance problem with editing the face of a cone
PR 6483986: Select - Fence Select -Taking 22 plus minutes to select

===Solid Edge Embedded Client===

PR 1830642: Latest Released rev rule is not honored when cache is not empty
PR 1827916: French AddToTeamcenter does not create JT datasets.
PR 6499716: SEEC_PDF_Dataset_Type preference does not work with non default PDF dataset
PR 6515493: Find No warning message appears twice
PR 6516857: Problem with property values driven by LOV and the PreCPD event API


---
End
---