Solid Edge ST7 SDK
Solid Edge ST3 MP8 - Readme

--------------
Legal Notices
--------------
©2011 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        103.00.08.06
Date:           07-Sep-2011

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
103.00.00.114, 103.00.01.05, 103.00.02.04, 103.00.03.04, 103.00.04.05,
103.00.05.03, 103.00.06.05, or 103.00.07.05.

This release of Solid Edge has been certified to run on the following:

- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit)
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit)
- Internet Explorer 8 (IE 6.0 meets minimum requirements)
 
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===

PR 1844579: Need Automation support for creating PMI dimensions
PR 6585353: BalloonDisplayedText API does not return the correct info

===Assembly===

PR 6560593: A large number of embedded weldment bodies causes performance issues for view rotation
PR 1848704: Getting an error when adding a new standard part (from existing part file)
PR 1854670: Assembly aborts when using Interpart Manager
PR 1855154: Unable to import a Solid Works-asm (SW2010)
PR 1859600: Assembly contains parts that no longer display after adding Assembly Features
PR 2174262: Unable to place a 15 degree fitting, while all other angles can be placed
PR 6576033: pathfinder reports erroneous driven parts for top level sketches
PR 1855845: Text font size doesn't change on sketch dimensions
PR 6571258: significant performance hit when profile has extra points
PR 6487257: STEP file import performance is very slow using this file
PR 1857542: Piping Performance is bad on ST3MP6 XP32BIt compared to V20 XP32Bit
PR 2175526: Problems with fitting positioning on piping
 
===Draft===

PR 1846417: Ordinate dimensions changed after opening in ST3
PR 6578739: Solid Edge aborted on close
PR 2174989: drawing view caption is moving on file open
PR 2175139: specific edges are not displayed when the draft file is opened
PR 1794331: a trim operation has a delay of 1 min+ in this file
PR 2175819: Parts List marks ambiguous parts even though the option is disabled
PR 6557936: PDF sheet sizes are swapped
PR 1861764: Performance problem updating a view after many additions/deletions in the model
PR 6572180: Spell Checker changes justification and removes text
   Note: The updated spell checker can be downloaded from:
         http://ftp.ugs.com/solid_edge/SupportTools/SpellChecker/

===Insight/View & Markup===

PR 1844744: No error displayed when search query ends 10x with timeout
PR 6557429: Crash editing sync file in asm after synchronizing through Cache Assistant
PR 1856783: any user can release assemblies that contain parts with a Prerelease or Obsolete status
PR 6569695: Revise and set path operation creates duplicate files
PR 6571007: Full Text search hangs on WSS3 server
PR 6424248: User cannot create a revision as a member of a domain group
PR 2165916: Traditional Chinese View & Markup aborts closing files
   Note: A workaround / partial fix for PR#2165916 has been verified for MP8 that
         requires you to manually delete FrameBrokerWeb_res.dll & WorkspaceManager_res.dll
         files. The complete fix is scheduled for ST5.

===Part/Profile/Sheet Metal===

PR 1857983: Synchronous hole thread disappearing when an ordered cutout is placed on the sheet metal part
PR 6566839: Doing a recompute on first feature and Solid Edge hangs
PR 1856721: Select from sketch features indicate under-constrained profiles
PR 1860323: DIN.PZL and neutral factor has no impact on converted sheetmetal parts
PR 6576500: Fewer Undo steps after each sketch, ending with a system error
PR 1861355: Product Aborts when saving or loading a customization file with "deny" security
PR 1860681: Unable to edit dimensions in a sketch
PR 6580444: Bends w/default bend radius are not driven by the global setting after transform
PR 6582077: Adding a cutout makes part disappear
PR 1856611: Part disappears after move/zoom/rotate

===Solid Edge Embedded Client===

PR 6569840: cannot save searches based on newly created searches
PR 1843322: NX part files are not updated / removed from SEEC cache
PR 1851218: Very low performance for AddToTeamcenter
PR 1851237: Solid Edge Item Number Sync works not from TC to SE
PR 6515479: Find Number for TcVC tries to reset and can lead to a collision
PR 6546565: Sets Priority ID for a new revision of a part in the CPD and it changes Priority id


---
End
---