Solid Edge ST7 SDK
Solid Edge ST3 MP9 - Readme

--------------
Legal Notices
--------------
©2011 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        103.00.09.05
Date:           03-Nov-2011

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
103.00.00.114, 103.00.01.05, 103.00.02.04, 103.00.03.04, 103.00.04.05,
103.00.05.03, 103.00.06.05, 103.00.07.05, or 103.00.08.06.

This release of Solid Edge has been certified to run on the following:

- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit)
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit)
- Internet Explorer 8 (IE 6.0 meets minimum requirements)
 
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, unbundle the zip file and
then dbl click on exe to install the Maintenance Pack.

Windows 7 Installation tips: In addition to turning off UAC, right click on the exe
and select "run as administrator" to complete the installation.

Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing
Solid Edge somewhere other than the default “Program Files” folder. Install in a location
like c:\SolidEdge\ that the user has full permission to write to.


-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===

PR 6587188: User requests new event be fired when SE is minimized
PR 1852602: Replace part which belongs to a part family doesn't invoke OnFileOpenUI
PR 6579864: How to Select Pipe in Draft document
PR 6578131: Added automation method to get associated assembly occurrence from draft

===Assembly===

PR 1856366: Editing an assembly sketch takes long time
PR 6571860: Tabs in pathfinder disappear after returning from sketch
PR 6510787: Missing Sub Assemblies when translating the supplied STEP file
PR 6465764: Select tool does not pick foreground geometry first
PR 1840866: Pattern cannot be created in sync if asm feature cuts part of pattern definition
PR 1862217: Assembly pattern fails when assembly features are present
PR 2173976: Conflicting Relationships
PR 1867394: Wrong result if 'Ignore interference between matching threads' is activated
PR 6555905: Slow to open Part Library tab
PR 6584857: Assembly hole features not honoring number of holes in profile
PR 1863648: Improved performance when placing subassemblies.
PR 6570990: Fixed an abort at HReGenerateSlot
PR 1867986: Unable to delete button when macro not found
PR 1862159: Save As is not updating the 'last saved by' property

===Draft===

PR 2174883: Dimension moves on file open
PR 6573451: No longer able to place balloons so that item numbers are in sequence
PR 6588632: Display configurations not retained when you create a principal view
PR 1869499: Moments of inertia will not consider the scale Factor

===Insight/View & Markup===

PR 6462473: Schema modifications prevent SharePoint SPs and Patches from installing
PR 1859033: Property values incorrect using ATL on pre-ST3 files with special characters
PR 6406729: Cannot move a file within the obsolete folder
PR 1864164: Sheetmetal files contain incomplete property structures in the Material Data

===Part/Profile/Sheet Metal===

PR 6590407: The seiges.exe executable crashes
PR 1866125: Fixed reproducible crashes in ordered part with go to bluesurf
PR 2174860: The replace face command fails after recompute
PR 1860864: Dimensions, annotations, and constraints colored wrong after text profiles
PR 1866219: Crash while editing Keypoint-Curve
PR 1862217: legacy document Coordinate system is ignored during fit

===Solid Edge Embedded Client===

PR 1787480: Analyze Files does not report Broken Links
PR 1857407: Editing sub-assembly is longer when the top assembly is opened read-only
PR 1858220: UOM mapping problem in SEEC
PR 1865867: Cannot open SE dataset from RAC if previous SE session was unmanaged
PR 6558493: Working with texture and image bitmaps
PR 6595479: Open from MRU does not open from Tc but checks out the dataset
PR 6420435: Problem with graphic display in Teamcenter Feature Library tab

---
End
---