Solid Edge ST7 SDK
Solid Edge ST4 MP10 - What's New
Problem Reports
Item Description
PR 2208599 Can't use the StudyOwner.Count property in ST4
PR 1914096 GetReferenceToGraphicMember2 returns a runtime error
PR 1915928 When opening an alternate assembly with the API function an exception occurs
PR 1888771 Resolved issues with Ribbon Bar Customizing
PR 1911009 Split Button & Drop Button doesn't work for macros
PR 2205600 Changing Drawing View Style by API is strange when the views are made in V20
PR 2207742 NormalToFaceCutOuts.Add method does not return the expected result
New APIs
None
See Also