--------------
Legal Notices
--------------
©2011 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 104.00.02.05
Date: 17-Nov-2011
Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
This Maintenance Pack can be installed on top of Versions:
104.00.00.82 or 104.00.01.08
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, unbundle the zip file and
then dbl click on exe to install the Maintenance Pack.
Windows 7 Installation tips: In addition to turning off UAC, right click on the exe
and select "run as administrator" to complete the installation.
Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing
Solid Edge somewhere other than the default “Program Files” folder. Install in a location
like c:\SolidEdge\ that the user has full permission to write to.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
===API===
PR 1858168: Problem with the Add-in Menu, does not display correct the first time, works fine the second time
===Assembly===
PR 1863648: Drag & Drop performance depends of asm size and if components are hidden or not
PR 1867394: Wrong result if 'Ignore interference between matching threads' is activated
PR 6555905: Parts Library tab is slow to open when an Insight .par or .psm is last selected/highlighted in the tab
PR 6584857: Assembly hole features not honoring number of holes in profile
PR 1867986: Unable to delete button when macro not found
===Draft===
PR 6579864: Having problems selecting a Pipe in Draft document
PR 1867983: Parts List column Property Text is changing when ST2 file is opened in ST3 or 4
PR 6603842: Parts List maximum row setting is overwritten
PR 1868919: Diameter symbol in callout displayed as %DI in 3D pdf
PR 1869690: No options when saving .emf in draft environment
PR 6541132: Cannot Open NX8 Documents
PR 6599967: Solid Edge crash
PR 1869499: Moments of inertia will not consider the scale Factor
PR 1870486: Line up text with left alignment does not work properly
PR 6609433: Crash when placing drawing view after hitting back button in DV wizard
PR 1826842: Parts list is not exported when attribute layer mapping is on
PR 1842000: There is a gap between leader and break line of a callout in certain positions
===Part/Profile/Sheet Metal===
PR 1864164: Sheetmetal files contain incomplete property structures in the Material Data
PR 1869122: Automatic detection of add/remove wrong in this case
PR 1869195: add/ cut option automatically switches to add when selecting axis of revolution
PR 6599667: reduce time for processing result in Simulation
PR 6603049: Cannot enter value and units while in the Move command in ST4
PR 1862713: Holes with threads cannot be selected for adding relationships
PR 1867683: Rigid does not work for hole features
PR 6583151: Property overrides (simulation) is not taken into account
===Solid Edge Embedded Client===
PR 6420435: SEEC Problem with graphic display in Teamcenter Feature Library tab
---
End
---