Solid Edge ST7 SDK
Solid Edge ST4 MP8 - Readme

--------------
Legal Notices
--------------
©2012 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        104.00.08.08
Date:           21-Sep-2012

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
104.00.00.82, 104.00.01.08, 104.00.02.05, 104.00.03.05, 104.00.04.05,
104.00.05.05, 104.00.06.05, or 104.00.07.04.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, unbundle the zip file and
then dbl click on exe to install the Maintenance Pack.

Windows 7 Installation tips: In addition to turning off UAC, right click on the exe
and select "run as administrator" to complete the installation.

Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing
Solid Edge somewhere other than the default “Program Files” folder. Install in a location
like c:\SolidEdge\ that the user has full permission to write to.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===

PR 2188413: Geometry from addin unexpectedly being removed from UnDo on Next command
PR 1903366: Replace via API does not work as via User Interface
PR 1891179: GetGlobalParameter (..glMinimumFlatLength) always delivers 0.0025
PR 1875930: API - wrong Text Box Width and Weight when adding multi line text
PR 2201222: problem with the method of reading and changing the dimension style by API
PR 2201877: API: Parent Object of the fill pattern cannot be acquired

===Assembly===

PR 1901251: FOA file aborts on open
PR 1902643: Pattern fails to update correctly when used with family of assemblies
PR 2198695: Positioning of node in Frame Simulation always offsets from Line End 1
PR 1903074: QAT will be deleted after modification
PR 6608469: displaying subassembly parts.
PR 1900020: display issues after locating dimensions in Assemble
PR 1907507: Failing relationships when assembly features are recomputed in ST4
PR 2197077: Error - No License - WEBPUBLISHER
PR 6623403: Conflicting error message on feature compute.
PR 1903013: Missing override body information caused assembly features to not be visible
PR 1906702: Cannot place connect relation in some workflows
PR 1902264: A reproducible crash on redo after deleting assembly features
PR 6769819: Assembly file not shrinking as expected when components are deleted
PR 6769125: Multiple Solutions dialog one hour after updating all links
PR 2201912: Circle not locating properly when creating 3D segment in XpresRoute in sub-assembly
PR 6772627: Zones do not work properly with Adjustable Assemblies

===Draft===

PR 1879173: Subscript text size cannot be changed via stack options
PR 1904131: The command 'Retrieve Dimensions' generates a small angular dimension
PR 1904254: Fixed a problem aligning drawing views using keypoints to blocks
PR 1904828: Solid Edge Crash when Editing Text
PR 1905667: Merge vertical cells with same value doesn't work correctly
PR 1906483: Dimension's projection lines are not shown
PR 1906525: Underlined balloons added in ST4 to ST3 ones are orientated to the wrong side
PR 2198792: Dimension disappears when "Convert to 2D View" is executed
PR 2200501: Tolerance symbol removed when dimension is dragged in AutoCAD
PR 2202087: Scale line widths should be enabled by default instead of scale line types
PR 1906788: Fixed a problem with LT format code not displaying in Callout text on scalar values
PR 1910328: Stretch command does not work on shared embed inserted symbols
PR 6767274: Clicking Back or Cancel in the Drawing View Layout step causes a crash
PR 1911446: Save As PDF - No error message when pdf file couldn't be overwritten
PR 6759715: Center justified callout jumps to the left when modified
PR-6776073: New callouts with property text don't honor the user's return/new lines
PR 1909452: Dimensions detach or incorrectly bind on update of view with PMI sections

===Part/Profile/Sheet Metal===

PR 1903647: Thread information not being present in Synchronous part copy
PR 2198575: Can´t import CATIA V5 file
PR 2199611: After adding protrusion 'Edit Definition handles' does not appear for some holes
PR 2200996: the move faces command terminating if "Ctrl+F" is used
PR 6724478: Red Pencils in PathFinder after Edit Profile with no changes
PR 6735355: Part disappears when adding a pattern of holes
PR 6747704: Not seeing the failure code during preview
PR 1907418: Solid Edge is closing when using show variability
PR 2202748: Abort when using mouse wheel to scroll through MRU
PR 1902823: Differences in Flat Pattern between ST2 and ST4
PR 1904514: Wrong visualization when suppressing an occurrence in assembly sketch pattern

===Insight===

PR 1905478: Revision Manager Set Path Browse for Folder slow performance over network on Windows 7
PR 6758938: Bend Radius change is not honored in a SharePoint managed assembly

===Solid Edge Embedded Client===

PR 1884750: Diagnostics tool is not working
PR 1902765: Error on save as translated from read-only part opened from assembly.
PR 1905070: Data preparation - Filename with accents
PR 6730948: Setting the revision and then the Item ID causes the dataset name to not display
PR 6740151: Edge crashes on saving the file to Teamcenter sub folder and then exit
PR 6748390: Query will not return TC item revisions with no SE datasets
PR 6746704: BOM Dialog display for Empty Item Revision
PR 1903302: Revise with SEEC_Image_Generate_3D=false creates JT file if already present
PR 6721338: SEEC Admin Policy files are getting delivered to the wrong location
PR 6760443: Custom Property on draft file converting from date field to text field.
PR 1902441: Save As into existing item revision doesn't work (naming rule)
PR 1899293: Non SE datasets are loaded in ST Cache during load process
PR 1907261: Assigning Rev ID before Item ID in Save As incorrectly names dataset
PR 1901182: Property manager needs hour(s) to show properties


---
End
---