Solid Edge ST7 SDK
Solid Edge ST4 MP9 - Readme

--------------
Legal Notices
--------------
©2012 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        104.00.09.04
Date:           01-Nov-2012

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
104.00.00.82, 104.00.01.08, 104.00.02.05, 104.00.03.05, 104.00.04.05,
104.00.05.05, 104.00.06.05, 104.00.07.04, or 104.00.08.08.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, unbundle the zip file and
then dbl click on exe to install the Maintenance Pack.

Windows 7 Installation tips: In addition to turning off UAC, right click on the exe
and select "run as administrator" to complete the installation.

Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing
Solid Edge somewhere other than the default “Program Files” folder. Install in a location
like c:\SolidEdge\ that the user has full permission to write to.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===
PR 6775244: Unpinned add-in docking pane can have incorrect text displayed
PR 2205091: Normal cutout (NormalToFaceCutOuts.Add) API fails

===Assembly===
PR 6744240: Abort with the Transfer command
PR 6754673: Fixes a possible abort in the Drag Component command
PR 6763841: Solid Edge Termination while applying constraints in an assembly

===Draft===
PR 1913655: Not exporting colors when "Do Width to Color Mapping" option disabled.
PR 2167823: Save As PDF generates raster low res text.
PR 2204199: Crash when double click on the draft view properties Dialog
PR 2206141: When broken view is added, angular dimensions shows wrong value
PR 2206659: Draft aborts after applying "Fit to Content" to the textbox

===Part/Profile/Sheet Metal===
PR 6587180: Quick Access Toolbar customization is not saved

===Insight===
PR 6763879: Issue in renaming part file linked with draft file.
PR 1875521: SharePoint on different port that 80 - StdParts Configuration Wizard Error

===Solid Edge Embedded Client===
PR 1907081: Structure Editor Operation "Save as" clears "Item name" field
PR 2197385: If I double click the assembly at TC, it is opened abnormally
PR 2197573: There are differences of cache files count between Teamcenter and Solid Edge
PR 6778014: SEEC_UOM_List_as_Geometric is not delivered by Teamcenter Admin
PR 1893221: Structure synchronization required when loading legacy SE assemblies.
PR 1906966: Structure Editor "Save as" changes the source item revision name
PR 1911954: SEEC/MP7 French - Assembly Save As problem when a draft is linked to a 2nd Asm.
PR 6763520: ST4 MP06 - TC 8.3.3 - Solid Edge CPD missing defined LOVs.
PR 6771389: SEEC: Need to improve AtT messaging
PR 6741867: SESE: ItemID Not Generated Like RAC: USER_EXIT Customization
PR 6784021: LOV out of sync after Save As of related Part and Draft files
PR 6787242: ATT_VIEW_PASSFAILCSVFILE  registry entry not created until a file is imported
PR 6787270: No error given importing different file to the same item id

---
End
---