Solid Edge ST7 SDK
Solid Edge ST5 MP2 - Readme

--------------
Legal Notices
--------------
©2012 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        105.00.02.06
Date:           08-Nov-2012

Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Version:
105.00.00.102 or 105.00.01.15.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, unbundle the zip file and
then dbl click on exe to install the Maintenance Pack.

Windows 7 Installation tips: In addition to turning off UAC, right click on the exe
and select "run as administrator" to complete the installation.

Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing
Solid Edge somewhere other than the default “Program Files” folder. Install in a location
like c:\SolidEdge\ that the user has full permission to write to.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===SE Viewer/View & Markup===

PR 6699703: Solid Edge Viewer and or V&M will not work using an account without administrator privileges
PR 1912893: You get a "Failed to open document" message with Solid Edge Viewer if you are not administrator
PR 6755246: Warning message pops up when attempting to open Japanese files in V&M
PR 6755847: Cannot open this pcf file in V&M
PR 6755981: V&M cannot save this file as .pcf
PR 6761505: PCF files with double byte characters in file name cannot be opened by V&M
PR 6790006: Pre-ST3 pcf files prompt for password when opening in V&M
PR 2204400: Solid Edge files with double byte characters in file name cannot be opened by V&M
PR 6729766: Attempting to open a pcf file created in ST4 causes V&M to go into an infinite loop

===API===

PR 6780496: Clicking customize command results in docking pane flying out
PR 1911009: Customize -> Ribbon: Split Button & Drop Button doesn't work for macros
PR 2205091: Normal cutout (NormalToFaceCutOuts.Add) API fails
PR 2207742: NormalToFaceCutOuts.Add methd does not return the expected result

===Assembly===

PR 1912542: Save As function for 3D PDF corrupts memory
PR 1912486: Relationships are still applied when Maintain Relationships is turned off
PR 6731912: Standard Parts is not accessible after undo during placement while IPA
PR 6739203: horizontal/vertical face relate does not allow keypoint selection in assembly
PR 6744240: Abort with the Transfer command
PR 6754673: Random abort in the Drag Component command
PR 6787689: Assembly Relationship tool crashes
PR 1914438: Empty Assembly takes is still 70MB
PR 6671120: When creating a pipe routes with Schedule 40 piping it will place a Schedule 10
PR 6726819: Mirror creates multiple occurrences when the target has multiple instances
PR 6781360: Crash while editing XpresRoute path
PR 1904399: Assembly hole feature will have the wrong diameter if profile is copy/pasted
PR 2207472: Captured fit lost on conversion to ST5

===Draft===

PR 6780184: Bring to Front and Send To Back no longer in Customize for Draft
PR 1909883: Icon wrong for user-defined plane when edited
PR 2167823: Save As PDF generates low resolution raster text
PR 2206141: When broken view is added, angular dimensions shows wrong value
PR 2206659: Draft aborts after applying "Fit to Content" to the textbox
PR 6784794: It takes 20 seconds to switch sheets
PR 6787216: Precision of primary linear tolerance is resetting to 2 decimal places
PR 1916758: Reattached Center marks caused projection lines to disappear
PR 1913819: Smart Dimension directionally challenged when zoomed in
PR 1917507: Scale- primary caption will not be shown since ST4, regression against ST3
PR 6794152: Weld Symbols in color are printing in color when set to black.
PR 1914664: SEEC Save as 3D PDF corrupts subsequent draft auto generated 2D PDF files
PR 1916499: Crash after pasting into block view
PR 2203988: Starting point of dimension's projection line shifts

===Part/Profile/Sheet Metal===

PR 6785458: Disallow save of files after a crash based on a registry switch
PR 6778308: Cannot place a tapered thread feature
PR 1909877: Cannot move holes in example part placed on a cylinder using “A” Alignment
PR 1911799: problem with synchronous Inter-Part
PR 1912822: Pattern of holes on top of smaller cylindrical cutout creates invalid body
PR 6739275: Radial pattern of a cutout fails to place all occurrences
PR 6746461: Multiple faces highlight when multiple persisted relationships share a face
PR 6767601: open surface will not unite with a solid
PR 6779245: Opening an Inventor Assembly is opening all parts as Ordered
PR 1914930: "M" key (to align to a midpoint) causes a difference in alignment
PR 6763967: Dimension edit in one direction with suspend Live Rules results in symmetric edit
PR 6776982: Dimension behaves as locked when first placed and conflicts with itself
PR 1915496: Edit fails because of relaxed dimension that should allow the change
PR 1915677: Part aborts placing male thread on chamfered cylinder
PR 6787757: Using undo twice causes face relationship to fail
PR 6789091: Removal of bend CPF constructions not happening correctly
PR 2206976: 3D measure command does not maintain the size and place of the results dialog
PR 6791469: In ST4 the user could create a flat pattern using the unbend in ST5 they can not
PR 6793940: Unable to select the construction body as a target body for subtract and split
PR 1917066: Assembly aborts using 3D Input Device from 3DConnexions

---
End
---