--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 100.00.03.03
Date: 15-Jan-2009
This Maintenance Pack can be installed on top of Version:
100.00.00.133, 100.00.01.07, or 100.00.02.07.
Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
=====Assembly=====
PR 1702197: Animation Editor Timeline crashes Solid Edge
PR 1515114: Pattern of a family member is not created correctly in this assembly
PR 1693966: Out of context tube still updates after a Save As of the assembly
PR 2097365: Variable renamed by user in V19 is not being displayed with variable table filter
PR 5918252: Pattern is not updating in this file when Height is set to original value
PR 6018360: Solid Edge hangs when changing placement options while placing angular relationships
PR 6061245: Column designer is calculating the wrong area moments of inertia for I-beams
PR 6063339: Opening a sub-assembly and then IPA into Part shows the wrong tree in Pathfinder
PR 6066064: Cannot locate pattern along curve reference feature
PR 6073010: Reorder not working when in place activated
PR 6075425: No Cancel or Finish buttons were displayed in assembly feature pattern CommandBar.
PR 6075436: Smart/Fast pattern buttons moving around in CommandBar.
=====Part/Profile/Sheetmetal=====
PR 1701884: Solid Edge aborts when opening Advances Units in File Properties
PR 2111593: Strange lines appear in this Draft file
PR 6027495: Save As to ACIS is moving the version up 4 from the version selected
PR 6075309: XpresRoute floating license not functioning properly
PR 6012839: Simplify B-splines is not working in certain files
PR 2113007: Solid Edge aborts when dismissing the default layer properties dialog
=====Draft=====
PR 1683725: Unable to drive the position of a text profile with dimensions
PR 1698339: Solid Edge aborts when fit is performed in this Draft file
PR 2070745: The display of the value of a "Chamfer Dimension" is shifted
PR 2110529: "Dimension value" is lying on top of "Dimension line"
PR 2111938: ACAD multiple text color is not imported
PR 5938516: Weld Symbol Properties dialog missing General tab at times
PR 6050476: Layer names are mistranslating
PR 6064282: Angular dimensions are incorrect when saving to AutoCAD
---
End
---