Solid Edge Assembly Type Library
AddNormalToCurveAtArcLengthRatio Method
Specifies the plane to which the operation is oriented.
Specifies the arc length ratio.
Specifies the x-axis rotation angle.
Member of the ReferenceElementConstants constant set that specifies the normal orientation.
Member of the ReferenceElementConstants constant set that specifies the curve end.
Description
Adds a reference plane normal to a curve at the specified arc length ratio.
Syntax
Visual Basic
Public Function AddNormalToCurveAtArcLengthRatio( _
   ByVal Parent As Object, _
   ByVal OrientationPlane As Object, _
   ByVal ArcLengthRatio As Double, _
   ByVal XAxisRotation As Double, _
   ByVal normalOrientation As ReferenceElementConstants, _
   ByVal arcLengthRatioOrigin As ReferenceElementConstants _
) As AsmRefPlane
Parameters
Parent
OrientationPlane
Specifies the plane to which the operation is oriented.
ArcLengthRatio
Specifies the arc length ratio.
XAxisRotation
Specifies the x-axis rotation angle.
normalOrientation
ValueDescription
ig3PointPlane
igAngular
igAtAngleToSurfaceAtKeypoint
igCurveEnd
igCurveStart
igFlipNormal
igNormalSide
igNormalToCurve
igNormalToCurveAtArcLengthRatio
igNormalToCurveAtDistance
igNormalToCurveAtDistanceAlongCurve
igNormalToCurveAtKeyPoint
igParallel
igParallelThroughPointUnsupported Internal type.
igPivotEnd
igPivotStart
igPlaneAlignX
igPlaneAlignY
igPlaneByMirror
igPlaneFlipHorizontal
igPlaneFlipVertical
igPlaneRotateLeft
igPlaneRotateRight
igRefEleInit
igReverseNormalSide
igTangentToFace
igTangentToSurfaceAtAngle
igTangentToSurfaceAtKeypoint
Member of the ReferenceElementConstants constant set that specifies the normal orientation.
arcLengthRatioOrigin
ValueDescription
ig3PointPlane
igAngular
igAtAngleToSurfaceAtKeypoint
igCurveEnd
igCurveStart
igFlipNormal
igNormalSide
igNormalToCurve
igNormalToCurveAtArcLengthRatio
igNormalToCurveAtDistance
igNormalToCurveAtDistanceAlongCurve
igNormalToCurveAtKeyPoint
igParallel
igParallelThroughPointUnsupported Internal type.
igPivotEnd
igPivotStart
igPlaneAlignX
igPlaneAlignY
igPlaneByMirror
igPlaneFlipHorizontal
igPlaneFlipVertical
igPlaneRotateLeft
igPlaneRotateRight
igRefEleInit
igReverseNormalSide
igTangentToFace
igTangentToSurfaceAtAngle
igTangentToSurfaceAtKeypoint
Member of the ReferenceElementConstants constant set that specifies the curve end.
Remarks
This method creates a new reference plane normal to the specified curve. The new plane is created at a distance that is the percentage of the curve length along the curve.
See Also

AsmRefPlanes Collection  | AsmRefPlanes Members