Solid Edge Assembly Type Library
AddNormalToCurveAtKeyPoint Method
Specifies the parent curve for the operation.
Specifies the plane to which the operation is oriented.
Specifies a reference to a vertex on a part edge or curve through which the plane passes.
Specifies the x-axis rotation angle.
Member of the ReferenceElementConstants constant set that specifies the curve end.
Description
Adds a reference plane normal to a curve at the specified keypoint.
Syntax
Visual Basic
Public Function AddNormalToCurveAtKeyPoint( _
   ByVal Parent As Object, _
   ByVal OrientationPlane As Object, _
   ByVal Keypoint As Object, _
   ByVal XAxisRotation As Double, _
   ByVal normalOrientation As ReferenceElementConstants, _
   ByVal selectedCurveEnd As ReferenceElementConstants _
) As AsmRefPlane
Parameters
Parent
Specifies the parent curve for the operation.
OrientationPlane
Specifies the plane to which the operation is oriented.
Keypoint
Specifies a reference to a vertex on a part edge or curve through which the plane passes.
XAxisRotation
normalOrientation
ValueDescription
ig3PointPlane
igAngular
igAtAngleToSurfaceAtKeypoint
igCurveEnd
igCurveStart
igFlipNormal
igNormalSide
igNormalToCurve
igNormalToCurveAtArcLengthRatio
igNormalToCurveAtDistance
igNormalToCurveAtDistanceAlongCurve
igNormalToCurveAtKeyPoint
igParallel
igParallelThroughPointUnsupported Internal type.
igPivotEnd
igPivotStart
igPlaneAlignX
igPlaneAlignY
igPlaneByMirror
igPlaneFlipHorizontal
igPlaneFlipVertical
igPlaneRotateLeft
igPlaneRotateRight
igRefEleInit
igReverseNormalSide
igTangentToFace
igTangentToSurfaceAtAngle
igTangentToSurfaceAtKeypoint
Specifies the x-axis rotation angle.
selectedCurveEnd
ValueDescription
ig3PointPlane
igAngular
igAtAngleToSurfaceAtKeypoint
igCurveEnd
igCurveStart
igFlipNormal
igNormalSide
igNormalToCurve
igNormalToCurveAtArcLengthRatio
igNormalToCurveAtDistance
igNormalToCurveAtDistanceAlongCurve
igNormalToCurveAtKeyPoint
igParallel
igParallelThroughPointUnsupported Internal type.
igPivotEnd
igPivotStart
igPlaneAlignX
igPlaneAlignY
igPlaneByMirror
igPlaneFlipHorizontal
igPlaneFlipVertical
igPlaneRotateLeft
igPlaneRotateRight
igRefEleInit
igReverseNormalSide
igTangentToFace
igTangentToSurfaceAtAngle
igTangentToSurfaceAtKeypoint
Member of the ReferenceElementConstants constant set that specifies the curve end.
Remarks
This method creates a new reference plane normal to the specified curve. The new plane is created to pass through the specified keypoint.
See Also

AsmRefPlanes Collection  | AsmRefPlanes Members