Solid Edge Assembly Type Library
SetGlobalParameter Method
Specifies the global parameter for which the setting is to be set. Valid values are members of the ApplicationGlobalConstants for Application objects, AssemblyGlobalConstants for AssemblyDocument objects, PartGlobalConstants for PartDocument objects, SheetMetalGlobalConstants for SheetMetalDocument objects, or WeldmentGlobalConstants for WeldmentDocument objects.
Specifies the setting of the global parameter identified by the Parameter argument. The data type depends on the data being set. For Application objects, the data type is Long or Variant. For all other objects, the data type is Double.
Description
Sets the value of a specified global parameter for the referenced Application or document object.
Syntax
Visual Basic
Public Sub SetGlobalParameter( _
   ByVal Parameter As AssemblyGlobalConstants, _
   ByVal Value As Variant _
) 
Parameters
Parameter
ValueDescription
seAssemblyGlobalAutomaticUpdate
seAssemblyGlobalDefaultAccuracyForPartDensity
seAssemblyGlobalDefaultPartDensity
seAssemblyGlobalTubeBendRadius
seAssemblyGlobalTubeEndTreatmentAngle
seAssemblyGlobalTubeEndTreatmentDepth
seAssemblyGlobalTubeEndTreatmentInsideDiameter
seAssemblyGlobalTubeEndTreatmentOutsideDiameter
seAssemblyGlobalTubeEndTreatmentRadius
seAssemblyGlobalTubeMinimumFlatLength
seAssemblyGlobalTubeOuterDiameter
seAssemblyGlobalTubeWallThickness
seAssemblyGlobalWireHarnessDefaultBundleAdder
seAssemblyGlobalWireHarnessDefaultBundleClearance
seAssemblyGlobalWireHarnessDefaultCableAdder
seAssemblyGlobalWireHarnessDefaultHoleClearance
seAssemblyGlobalWireHarnessDefaultSlackCompensation
seAssemblyGlobalWireHarnessDefaultWireAdder
Specifies the global parameter for which the setting is to be set. Valid values are members of the ApplicationGlobalConstants for Application objects, AssemblyGlobalConstants for AssemblyDocument objects, PartGlobalConstants for PartDocument objects, SheetMetalGlobalConstants for SheetMetalDocument objects, or WeldmentGlobalConstants for WeldmentDocument objects.
Value
Specifies the setting of the global parameter identified by the Parameter argument. The data type depends on the data being set. For Application objects, the data type is Long or Variant. For all other objects, the data type is Double.
Remarks
The values for Arc quality (seApplicationGlobalDisplayArcQuality constant) range from 6 to 72. For values less than six, the display arc quality will be set to six. For values greater than 72, the display arc quality is set to 72. The values for Display Quality (seApplicationGlobalDisplayQuality) range from 0 to 48. For values less than 0, the display quality will be set to 0. For values greater than 48, the display quality will be set to 48.
See Also

AssemblyDocument Object  | AssemblyDocument Members