Solid Edge Assembly Type Library : AssemblyFeaturesHole Object |
![]() | Deletes the referenced object. |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | This method returns the profiles associated with the referenced feature object. |
![]() | |
![]() | |
![]() | Returns the high and low range values for the referenced object. |
![]() | This method rolls the referenced object back to a specified feature. |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | Sets the profiles associated with the referenced feature object. |
![]() | |
![]() |
![]() | |
![]() | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. The result of the Edges property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. |
![]() | |
![]() | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. The result of the Faces property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. |
![]() | Returns a collection of faces that are intersected by a specified vector. |
![]() | |
![]() | |
![]() | Returns the name of the referenced object. |
![]() | |
![]() | Temporarily suppresses the referenced object. |