Imports System.Runtime.InteropServices
Public Class Recompute
Private Sub Button1_Click(sender As System.Object, e As System.EventArgs) Handles Button1.Click
Dim objApplication As SolidEdgeFramework.Application = Nothing
Dim objType As Type = Nothing
Dim objAssemblyDoc As SolidEdgeAssembly.AssemblyDocument = Nothing
Dim objAssemblyFeatures As SolidEdgeAssembly.AssemblyFeatures = Nothing
Try
' Create/get the application with specific settings
objApplication = Marshal.GetActiveObject("SolidEdge.Application")
If objApplication Is Nothing Then
' Get the type from the Solid Edge ProgID
objType = Type.GetTypeFromProgID("SolidEdge.Application")
' Start Solid Edge
objApplication = Activator.CreateInstance(objType)
' Make Solid Edge visible
objApplication.Visible = True
End If
'Get reference to active assembly document
objAssemblyDoc = objApplication.ActiveDocument
objAssemblyFeatures = objAssemblyDoc.AssemblyFeatures
objAssemblyFeatures.Recompute(0)
Catch ex As Exception
MsgBox(ex.ToString)
End Try
End Sub
End Class