Solid Edge Assembly Type Library : AssemblyStitchWeld Object |
![]() | |
![]() | |
![]() | |
![]() | Sets and returns the length of material to remove from the end of the weld bead for the referenced AssemblyStitchWeld object. |
![]() | Sets and returns the gap length between solid portions of the bead for the referenced StitchWeld object. |
![]() | Returns the name of the referenced object. |
![]() | |
![]() | Sets and returns the length of material to remove from the start of the weld bead for the referenced AssemblyStitchWeld object. |
![]() | Temporarily suppresses the referenced object. |
![]() | Specifies the type of the object being referenced. |
![]() | Specifies whether or not the referenced object is displayed to the screen. |