Solid Edge Assembly Type Library : Bundle Object |
![]() | |
![]() | Deletes the referenced object. |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | This method returns the start and end points of the referenced object. |
![]() | |
![]() | |
![]() | |
![]() | |
![]() |
![]() | Returns the active application object. |
![]() | Returns the AssemblyProperty object used to store path attributes for the referenced object. |
![]() | Returns the AttributeSets collection object for the referenced object. |
![]() | This read-write property sets or returns the color in which the active object is drawn. The color is stored as a long integer and is created with the RGB function (red, green, and blue color intensities) or as an integer between 0 and 16 that represents standard colors. |
![]() | |
![]() | |
![]() | Returns True if a specified Attribute Set exists on the referenced object. |
![]() | |
![]() | |
![]() | |
![]() | Returns the name of the referenced object. |
![]() | Sets and returns the outer diameter of the referenced object. |
![]() | Returns the parent object for the referenced object. |
![]() | |
![]() | |
![]() | Specifies the type of the object being referenced. |
![]() | |
![]() | Specifies whether or not the referenced object is displayed to the screen. |