| Solid Edge Assembly Type Library : CurveSegment Object |
AddPathSegment | Adds a path segment. |
Delete | Deletes the referenced object. |
GetPathSegment | Returns the input object specified by the index. |
HidePathSegments | Hides the input path segments. |
RemovePathSegment | Removes a path segment. |
ShowPathSegments | Shows the input path segments. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
EndDerivativeMagnitude | Sets and returns the end derivative magnitude. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Parent | Returns the parent object for the referenced object. |
PathSegmentsCount | Returns the number of input path objects. |
StartDerivativeMagnitude | Sets and returns the start derivative magnitude. |
Type | Specifies the type of the object being referenced. |
Validation | Determines curve validity. |
WhichKeypoints | Specifies the keypoints used to compute the curve. |