Solid Edge Assembly Type Library
Name Property
Description
Returns the name of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Name As String
Remarks
All objects have names that are unique within the scope of their parent.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objLayouts As SolidEdgeAssembly.Layouts
    Dim objLayout As SolidEdgeAssembly.Layout
    ' Local variables to be declared here
    Dim strName As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Layouts Collection
    Set objLayouts = objDoc.Layouts
    'Create a new Layout
    Set objLayout = objLayouts.Add(AsmRefPlane:=objDoc.RefPlanes(1))
    'Get the Name of the Layout
    strName = objLayout.Name
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLayouts = Nothing
    Set objLayout = Nothing
End Sub
See Also

Layout Object  | Layout Members