Solid Edge Assembly Type Library
ReorderOccurrence Method
The occurrence to be reordered.
The occurrence around which OccurrenceToReorder will be reordered.
Specifies whether OccurrenceToReorder is reordered before or after the target occurrence.
Description
Reorders an occurrence before or after the specified occurrence.
Syntax
Visual Basic
Public Sub ReorderOccurrence( _
   ByVal OccurrenceToReorder As Object, _
   ByVal TargetOccurrence As Object, _
   ByVal AfterTarget As Boolean _
) 
Parameters
OccurrenceToReorder
The occurrence to be reordered.
TargetOccurrence
The occurrence around which OccurrenceToReorder will be reordered.
AfterTarget
Specifies whether OccurrenceToReorder is reordered before or after the target occurrence.
See Also

Occurrences Collection  | Occurrences Members