Solid Edge Assembly Type Library
GetElement1 Method
Specifies whether the returned object is a TopologyReference.
Description
Returns the first element in this relationship.
Syntax
Visual Basic
Public Function GetElement1( _
   ByRef IsTopologyReference As Boolean _
) As Object
Parameters
IsTopologyReference
Specifies whether the returned object is a TopologyReference.
Remarks
This method returns TopologyReference information for the first of two elements constrained by the relationship.
See Also

PlanarRelation3d Object  | PlanarRelation3d Members