Solid Edge Assembly Type Library
NormalsAligned Property
Description
Indicates the manner in which the planar constraint on the referenced object was placed.
Property type
Read-write property
Syntax
Visual Basic
Public Property NormalsAligned As Boolean
Remarks
If the parts are aligned, NormalsAligned is True. If the parts are mated, NormalsAligned is False.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPlanarRel As SolidEdgeAssembly.PlanarRelation3d
    Dim bNormals As Boolean
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly document
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a planar relation object from the assembly document
    Set objPlanarRel = objDoc.Relations3d.Item(3)
    ' checking whether the normals are aligned
    bNormals = objPlanarRel.NormalsAligned
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPlanarRel = Nothing
End Sub
See Also

PlanarRelation3d Object  | PlanarRelation3d Members