Solid Edge Assembly Type Library
Status Property
Description
Returns the status (a member of the Relation3dStatusConstants constant set) of the referenced Part.
Property type
Read-only property
Syntax
Visual Basic
Public Property Status As Relation3dStatusConstants
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPlanarRel As SolidEdgeAssembly.PlanarRelation3d
    Dim lngStatus As Long
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly document
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a planar relation object from the assembly document
    Set objPlanarRel = objDoc.Relations3d.Item(3)
    ' getting the status of the relation
    lngStatus = objPlanarRel.Status
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPlanarRel = Nothing
End Sub
See Also

PlanarRelation3d Object  | PlanarRelation3d Members