Solid Edge Assembly Type Library
Type Property
Description
A member of the ObjectType constant set.
Property type
Read-only property
Syntax
Visual Basic
Public Property Type As ObjectType
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPointRel As SolidEdgeAssembly.PointRelation3d
    Dim lngType As Long
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly document
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a point relation
    Set objPointRel = objDoc.Relations3d.Item(9)
    ' getting the type of the relation
    lngType = objPointRel.Type
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPointRel = Nothing
End Sub
See Also

PointRelation3d Object  | PointRelation3d Members