Solid Edge Assembly Type Library : RigidSetRelation3d Object |
![]() | Adds an occurrence to the rigid set. |
![]() | Deletes the referenced object. |
![]() | Removes an occurrence from the rigid set. |
![]() | Selects the referenced object in the active window. |
![]() | Returns the active application object. |
![]() | Returns the AttributeSets collection object for the referenced object. |
![]() | Returns the detailed status of the Relation3d object. |
![]() | Returns the numeric index for the active object. |
![]() | Returns True if a specified Attribute Set exists on the referenced object. |
![]() | Returns whether or not an occurrence is a member of the rigid set. |
![]() | Returns the number of occurrences in the rigid set. |
![]() | Returns the occurrences that are members of the rigid set. |
![]() | Returns the parent object for the referenced object. |
![]() | Returns the status of the specified object. |
![]() | Temporarily suppresses the referenced object. |
![]() | Specifies the type of the object being referenced. |