Solid Edge Assembly Type Library
Angle Property
Collapse All
Expand All
Solid Edge Assembly Type Library
>
SegmentAngularRelation3d Object
: Angle Property
Description
Sets and returns the angular rotation of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Angle As Double
Remarks
For Rectangles, this value represents the rotation of the entire object. The angle is represented in Radians.
See Also
SegmentAngularRelation3d Object
|
SegmentAngularRelation3d Members