Solid Edge Assembly Type Library : StructuralFrame Object |
![]() | Frames created in ST3 are associative to cross section part files. i.e. If part file modifies, frame in assembly updates. To avoid this for legacy frames (frames created prior to ST3), user can use this API. |
![]() | |
![]() | Deletes the construction surfaces from the frame. |
![]() | This method returns the frame path for the referenced StructuralFrame object. |
![]() | |
![]() | This method returns the global end condition for the referenced StructuralFrame object. |
![]() | This method returns the override end condition for the specified sections for the referenced StructuralFrame object. |
![]() | |
![]() | This method returns the part document in which the specified section resides for the referenced StructuralFrame object. |
![]() | This method returns the placement for the specified section for the referenced StructuralFrame object. |
![]() | This method returns the cross sections for the referenced StructuralFrame object. |
![]() | |
![]() | Retrieves the construction surfaces representing the hole locations from the cross section component file. These surfaces can be used to create holes as per the standard at appropriate locations in the frames. |
![]() | |
![]() | |
![]() | |
![]() | This method sets the frame path for the referenced StructuralFrame object. |
![]() | This method sets the global end condition for the referenced StructuralFrame object. |
![]() | This method sets the override end condition for the specified sections for the referenced StructuralFrame object. |
![]() | This method sets a new part document for the specified section for the referenced StructuralFrame object. |
![]() | This method sets a new placement for the specified section for the referenced StructuralFrame object. You must specify at least one optional parameter (Rotation, XDistance, or YDistance). |
![]() | Returns the active application object. |
![]() | Specifies the automatic positioning setting for the referenced StructuralFrame object. |
![]() | This read-write String property sets and returns the global document for the referenced StructuralFrame object. |
![]() | Returns the name of the referenced object. |
![]() | Returns the active application object. |
![]() | If a frame contains collinear paths, we can control whether to create single frame occurrence for collinear paths or not using this property. |
![]() | If a frame contains tangential paths, we can control whether to create single frame occurrence for collinear paths or not using this property. |
![]() | Controls the display of the referenced object. |