Solid Edge Draft Type Library : ConnectorTable Object |
ConvertToTable | Convert Connector Table to Table. |
CopyToClipboard | Copies the referenced ConnectorTable object to the operating system clipboard. |
Delete | Deletes the referenced object. |
GetListOfSavedSettings | Gets list of available saved settings. |
GetOrigin | Set the origin position of the Connector Table. |
SetOrigin | Sets the origin position of the Table. |
Update | Updates the referenced object. |
AdditionalSheetsBackgroundName | Gets or sets the name of background sheet for additional pages. |
AnchorPoint | Specifies which corner of the Table is the origin. |
Application | Returns the active application object. |
Cell | Gets the cell object which is the intersection of a row and column. |
ColumnHeaderPosition | Gets or sets column header position. |
Columns | Gets the columns collection |
CreateNewSheetsForTable | Gets or sets the option to create new sheets for each page. |
DataFixedRowHeight | Gets or sets fixed row height for data rows. |
DrawingView | Returns the DrawingView object for the referenced object. |
EnableGroups | Gets or sets teh option to enable groups. |
FillEndOfTableWithBlankRows | Gets or sets the option to fill end of page with blank rows. |
FirstSheetBackgroundName | Gets or sets the name of background sheet for first page. |
GroupByColumn | Gets or sets the column to group by. |
Groups | Gets the groups collection. |
HeaderFixedRowHeight | Gets or sets fixed row height for column header rows. |
IsUpToDate | Specifies whether or not the Connector Table is up to date with respect to the 3d model it references. |
MaintainSheetsWithTableSize | Gets or sets the option to delete sheet when page is removed. |
Margin | Gets or sets the margin between the text and cell border. |
MaximumHeightAdditionalPages | Gets or sets the maximum height of additional pages. |
MaximumHeightFirstPage | Gets or sets the maximum height of first page. |
MaximumRowsAdditionalPages | Gets or sets the maximum height of additional pages. |
MaximumRowsFirstPage | Gets or sets the maximum rows on first page. |
NumberOfHeaderRows | Gets or sets the number of header rows. |
PageGap | Gets or sets the gap between pages. |
Pages | Gets the pages collection. |
Parent | Returns the parent object for the referenced object. |
ReverseDisplayOrder | Gets or sets the option to reverse display order within each page. |
Rows | Gets the rows collection. |
SavedSettings | Returns the saved settings for the referenced object. |
ShowColumnHeader | Gets or sets the option to show column headers. |
ShowSheetBackground | Gets or sets the option to show the background sheet. |
TableStyle | Gets or sets the table style. |
TitleFixedRowHeight | Gets or sets fixed row height for title rows. |
Titles | Gets the titles collection. |
WrapDataCellsToNewRow | Gets or sets the option to wrap data cells to new row. |