Solid Edge Draft Type Library
CoordinateSystem2d Object Members
Overview 
Public Methods
Public Method GetAxisPropertiesReturns alignment axis information for the referenced CoordinateSystem2d object.
Public Method GetOriginReturns the origin for the referenced object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property IsDefaultSpecifies whether the referenced CoordinateSystem2d object represents the default coordinate system (True) or a user-defined coordinate system (False).
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property TypeSpecifies the type of the object being referenced.
See Also

CoordinateSystem2d Object