Solid Edge Draft Type Library
Orientation Property
Collapse All
Expand All
Solid Edge Draft Type Library
>
DVEllipse2d Object
: Orientation Property
Description
Sets and returns the direction in which an arc or elliptical arc is drawn.
Property type
Read-only property
Syntax
Visual Basic
Public Property Orientation As
Geom2dOrientationConstants
Remarks
This direction is in respect to the major axis and is either clockwise or counterclockwise. Valid values are members of the Geom2dOrientationConstants constant set.
See Also
DVEllipse2d Object
|
DVEllipse2d Members