Solid Edge Draft Type Library
DVLine2d Object Members
Overview 
Public Methods
Public Method GetEndPointReturns the coordinates of the end point of the referenced object.
Public Method GetKeyPointReturns information about a specified key point.
Public Method GetReferenceKeyReturns a reference key for the edge in the model.
Public Method GetSegmentedStyleReturns the start point, end point, and linear style applied to a specified segment of a 2-D geometry object.
Public Method GetStartPointReturns the coordinates of the start point for the referenced object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Properties
Public Property AngleSets and returns the angular rotation of the referenced object.
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property BendAngleReturns the bend angle from the underlying sheet metal model.
Public Property BendQuantityNumber of bends for a divide bend.
Public Property BendRadiusReturns the bend radius from the underlying sheet metal model.
Public Property DocumentReturns the document to which the referenced object belongs.
Public Property DrawingViewReturns the DrawingView for this object.
Public Property EdgeTypeReturns the EdgeType for this object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property KeyReturns a key (a string) to find the object relative to its owning parents.
Public Property KeyPointCountReturns the number of keypoints/handles that are supported by the referenced object.
Public Property LengthSpecifies the length of the referenced object.
Public Property ModelMemberReturns the ModelMember for this object.
Public Property ModelWeldsReturns the ModelWelds collection object.
Public Property NameReturns the name of the referenced object.
Public Property ReferenceReturns a Reference object for this object.
Public Property RelationshipsReturns a collection of objects that are related to the referenced graphic object.
Public Property SegmentedStyleCountReturns the number of segmented styles defined for the referenced graphic object.
Public Property ShowHideEdgeOverrideGets or sets a show/hide override on an edge or segment.
Public Property TypeSpecifies the type of the object being referenced.
See Also

DVLine2d Object