Solid Edge Draft Type Library
DVLineString2d Object Members
Overview 
Public Methods
Public Method GetCentroidReturns the coordinates of the centroid of the referenced object.
Public Method GetKeyPointReturns information about a specified key point.
Public Method GetReferenceKeyReturns a reference key for the edge in the model.
Public Method GetSegmentedStyleReturns the start point, end point, and linear style applied to a specified segment of a 2-D geometry object.
Public Method GetVertexReturns the coordinates of the referenced object based on a specified index.
Public Method GetVerticesReturns an array of vertex coordinates in a dimensioning object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AreaReturns the area of the referenced object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property ClosedReturns True if the start and end points of the referenced object are coincident.
Public Property DocumentReturns the document to which the referenced object belongs.
Public Property DrawingViewReturns the DrawingView for this object.
Public Property EdgeTypeReturns the EdgeType for this object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property KeyReturns a key (a string) to find the object relative to its owning parents.
Public Property KeyPointCountReturns the number of keypoints/handles that are supported by the referenced object.
Public Property LengthSpecifies the length of the referenced object.
Public Property ModelMemberReturns the ModelMember for this object.
Public Property ModelWeldsReturns the ModelWelds collection object.
Public Property NameReturns the name of the referenced object.
Public Property ReferenceReturns a Reference object for this object.
Public Property SegmentedStyleCountReturns the number of segmented styles defined for the referenced graphic object.
Public Property TypeSpecifies the type of the object being referenced.
Public Property VertexCountReturns the number of vertices in the referenced object.
See Also

DVLineString2d Object