Solid Edge Draft Type Library
DVPoint2d Object Members
Overview 
Public Methods
Public Method GetKeyPointReturns information about a specified key point.
Public Method GetPointReturns the coordinates of the referenced Point2d object.
Public Method GetReferenceKeyReturns a reference key for the edge in the model.
Public Method GetSegmentedStyleReturns the start point, end point, and linear style applied to a specified segment of a 2-D geometry object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DocumentReturns the document to which the referenced object belongs.
Public Property DrawingViewReturns the DrawingView for this object.
Public Property EdgeTypeReturns the EdgeType for this object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property KeyReturns a key (a string) to find the object relative to its owning parents.
Public Property KeyPointCountReturns the number of keypoints/handles that are supported by the referenced object.
Public Property ModelMemberReturns the ModelMember for this object.
Public Property NameReturns the name of the referenced object.
Public Property ReferenceReturns a Reference object for this object.
Public Property RelationshipsReturns a collection of objects that are related to the referenced graphic object.
Public Property SegmentedStyleCountReturns the number of segmented styles defined for the referenced graphic object.
Public Property TypeSpecifies the type of the object being referenced.
Public Property xSets and returns the x coordinate of the referenced Point2d object.
Public Property ySets and returns the y coordinate of the referenced Point2d object.
See Also

DVPoint2d Object