Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Caption | Sets and returns the caption of the referenced object. |
CaptionDefinitionText | Sets and returns the definition text for the caption. Definition text can contain codes for Property Text and Symbols. |
CaptionDisplayedText | Returns the text for the caption as displayed after processing Property Text and Symbols. |
DetailView | Returns the detail view associated with the detail envelope. |
Diameter | Sets and returns the diameter of the referenced object. |
DisplayAsCircle | Specifies whether to always display the detail envelope as a circle, even when the envelope's geometry is not a circle. |
DisplayCaption | Specifies whether or not the caption of the referenced object is displayed. |
DisplayStandard | Specifies the standard for displaying the detail envelope. |
DisplayViewSheetNumber | Sets and returns whether the ViewSheetNumber definition string is displayed in the caption. |
Document | Returns the document to which the referenced object belongs. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
Layer | Sets and returns the named layer on which the referenced object resides. |
LineType | Sets and returns the line display type of the drawing view. |
LineWidth | Sets and returns the line width (in paper space units) for the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Profile | Returns the profile associated with the parent object. |
SourceDrawingView | Returns the DrawingView object from which the detail drawing view is derived. |
StyleName | Sets and returns the name of the style that is applied to the referenced object. |
TextColor | Sets and returns the color of the text for the caption of the referenced object. |
TextFont | Sets and returns the text font of the caption of the referenced object. |
TextFontStyle | Sets and returns the text font style of the caption of the referenced object. |
TextHeight | Sets and returns the text height of the caption of the referenced object. |
TextRatio | Sets and returns the text ratio of the caption of the referenced object. |
Type | Specifies the type of the object being referenced. |
ViewSheetNumberDefinitionText | Sets and returns the View Sheet Number (%VN) definition string. This is intended for use with %{View Sheet Number|DV} property text and may include other formatting options. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |