Solid Edge Draft Type Library
Count Property
Description
Returns the number of objects in the referenced collection.
Property type
Read-only property
Syntax
Visual Basic
Public Property Count As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objModelLinks As SolidEdgeDraft.ModelLinks
    Dim objModelLink As SolidEdgeDraft.ModelLink
    Const TESTFILE = "T:\vbtests\testcases\chead.par"
    Dim lngCount As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the ModelLinks collection from the Document
    Set objModelLinks = objDoc.ModelLinks
    'Add a model to the Document
    Call objModelLinks.Add(Filename:=TESTFILE)
    'Get the number of Models attached to the Document with Count property
    lngCount = objModelLinks.Count
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModelLinks = Nothing
    Set objModelLink = Nothing
End Sub
See Also

ModelLinks Collection  | ModelLinks Members