Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objModelLink As SolidEdgeDraft.ModelLink
Dim objAttributeSets As Object
' Local variables to be declared here
Const TESTFILE = "T:\vbtests\testcases\chead.par"
Dim bAttribSetPresent As Boolean
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
On Error GoTo 0
'Get the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'Add a model to the Document
Set objModelLink = objDoc.ModelLinks.Add(Filename:=TESTFILE)
'Get the AttributeSets of line2d
Set objAttributeSets = objModelLink.AttributeSets
'Create an AttributeSet
Call objAttributeSets.Add("MyAttrib Set")
'Get IsAttributeSetPresent property
bAttribSetPresent = objModelLink.IsAttributeSetPresent("MyAttrib Set")
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objAttributeSets = Nothing
End Sub