Solid Edge Draft Type Library
ModelDocument Property
Description
Returns the document object of the source model file for the referenced ModelLink object.
Property type
Read-only property
Syntax
Visual Basic
Public Property ModelDocument As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objModelLink As SolidEdgeDraft.ModelLink
    Dim objModelLinkDocument As SolidEdgePart.PartDocument
    Const TESTFILE = "T:\vbtests\testcases\chead.par"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Add a model to the Document
    Set objModelLink = objDoc.ModelLinks.Add(Filename:=TESTFILE)
    'Get the Model's Document object used by ModelLink
    Set objModelLinkDocument = objModelLink.ModelDocument
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModelLink = Nothing
    Set objModelLinkDocument = Nothing
End Sub
See Also

ModelLink Object  | ModelLink Members