Solid Edge Draft Type Library
ModelType Property
Description
Returns the model type for the referenced ModelLink or ModelNode object.
Property type
Read-only property
Syntax
Visual Basic
Public Property ModelType As ModelLinkTypeConstants
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objModelLink As SolidEdgeDraft.ModelLink
    Const TESTFILE = "T:\vbtests\testcases\chead.par"
    Dim lngModelType As ModelLinkTypeConstants
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Add a model to the Document
    Set objModelLink = objDoc.ModelLinks.Add(Filename:=TESTFILE)
    'Get the Model's Type i.e., part/Assembly used by ModelLink
    lngModelType = objModelLink.ModelType
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModelLink = Nothing
End Sub
See Also

ModelLink Object  | ModelLink Members