Solid Edge Draft Type Library
UpdateViews Method
Description
Updates all views with the referenced model link.
Syntax
Visual Basic
Public Sub UpdateViews() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objModelLink As SolidEdgeDraft.ModelLink
    Const TESTFILE = "T:\vbtests\testcases\Part005.dft"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    objDoc.Close
    Set objDoc = objApp.Documents.Open(Filename:=TESTFILE)
    'Get the ModelLink associated with DFT file
    Set objModelLink = objDoc.ModelLinks(1)
    'Update All Drawing views associated with this ModelLink using UpdateViews method
    objModelLink.UpdateViews
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModelLink = Nothing
End Sub
See Also

ModelLink Object  | ModelLink Members