Solid Edge Draft Type Library
ModelNode Object Members
Overview 
Public Methods
Public Method GetAssemblyReferenceKeyReturns a key than can be used to refer to the corresponding assembly occurrence in the associated assembly document.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property ComponentName
Public Property CutLength
Public Property FileNameSets and Returns the file name of the referenced document.
Public Property IncludeInPartsListControls whether or not an occurrence is included in physical property calculations.
Public Property IsBalloonedReturns True if the referenced ModelNode object is ballooned in any of the drawing views contained in the draft document.
Public Property ItemNumberSpecifies the item number associated with the referenced ModelNode object.
Public Property ModelNodesReturns the ModelNodes collection object for the referenced ModelLink or ModelNode object.
Public Property ModelTypeReturns the model type for the referenced ModelLink or ModelNode object.
Public Property ParentReturns the parent object for the referenced object.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

ModelNode Object