Solid Edge Draft Type Library
TransparentDisplay Property
Description
Specifies whether or not transparent display is on.
Property type
Read-write property
Syntax
Visual Basic
Public Property TransparentDisplay As Boolean
Remarks
If True, all graphic objects on multiple-selected sheets are displayed; if False, only graphic objects on the active sheet are displayed.
See Also

SheetWindow Object  | SheetWindow Members