Solid Edge Draft Type Library
TableColumn Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property CurrentHeaderRowGets or sets the active header row for editing.
Public Property DataFitToWidthGets or sets whether to fit the column text to the width of the column.
Public Property DataFontNameGets or sets the font name of the text in the column.
Public Property DataFontStyleGets or sets the font style of the text in the column.
Public Property DataHorizontalAlignmentGets or sets the horizontal alignment of the text in the column.
Public Property DataMergeCellsWithSameValueGets or sets the option to merge cells with the same value.
Public Property DataUnderlineGets or sets the underline of the text in the column.
Public Property DataVerticalAlignmentGets or sets the vertical alignment of the text in the column.
Public Property HeaderRowFitToWidthGets or sets whether to fit the current header row text to the width of the column.
Public Property HeaderRowFontNameGets or sets the font name of the current column header row.
Public Property HeaderRowFontStyleGets or sets the font style of the current column header row.
Public Property HeaderRowHorizontalAlignmentGets or sets the horizontal alignment of the current header row text.
Public Property HeaderRowMergeWithNextGets or sets whether to merge the current column header with the next.
Public Property HeaderRowOrientationGets or sets the orientation of the header row.
Public Property HeaderRowUnderlineGets or sets the underline of the current column header.
Public Property HeaderRowValueGets or sets the current column header row contents.
Public Property HeaderRowVerticalAlignmentGets or sets the vertical alignment of the current header row text.
Public Property IndexReturns the numeric index for the active object.
Public Property ParentReturns the parent object for the referenced object.
Public Property PropertyTextGets or sets the column definition text. This is used as the template for filling out each row of this column.
Public Property ShowSpecifies whether or not the table is shown.
Public Property SortAscendingThis read-write Boolean property specifies that the selected data type in a Table Column object is to be sorted by ascending alphabetical order.
Public Property SortPrecedenceThis read-write Long property specifies whether the data type is to be used first, second, or third in determining sort order in a Table Column object.
Public Property WidthReturns the width of the referenced object.
See Also

TableColumn Object  | Solid Edge V19 - What's New