Solid Edge FrameworkSupport Type Library
AddAnnotAlignmentShape Method
Is an Array of X-coordinate of points.
Is an Array of Y-coordinate of points.
Description
This method defines Annotation Alignment Shape.
Syntax
Visual Basic
Public Function AddAnnotAlignmentShape( _
   ByRef ppPointsX() As Double, _
   ByRef ppPointsY() As Double _
) As AnnotAlignmentShape
Parameters
ppPointsX
Is an Array of X-coordinate of points.
ppPointsY
Is an Array of Y-coordinate of points.
Remarks
If first and last coordinates are same then closed type alignment shape will be placed.
Example
Imports System.Runtime.InteropServices

Public Class AddAnnotAlignmentShapes
    Private Sub btnAddAnnotationAlignmentShape_Click(sender As System.Object, e As System.EventArgs) Handles btnAddAnnotationAlignmentShape.Click
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objAnnotAlignmentShapes As SolidEdgeFrameworkSupport.AnnotAlignmentShapes = Nothing
        Dim objAnnotAlignmentShape As SolidEdgeFrameworkSupport.AnnotAlignmentShape = Nothing
        Dim dPointX(0 To 5) As Double
        Dim dPointY(0 To 5) As Double
        Dim dPointX1(0 To 5) As Double
        Dim dPointY1(0 To 5) As Double
        Dim dPointX2(0 To 5) As Double
        Dim dPointY2(0 To 5) As Double
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objLine As SolidEdgeFrameworkSupport.Line2d = Nothing
        Dim objCircle As SolidEdgeFrameworkSupport.Circle2d = Nothing
        Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
        Dim objAlignmentShape As SolidEdgeFrameworkSupport.AnnotAlignmentShape = Nothing
        Dim objType As Type = Nothing

        Try
            ' Create/get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If

            objDraftDoc = objApplication.ActiveDocument
            objSheet = objDraftDoc.ActiveSheet

            dPointX(0) = 0.0
            dPointX(1) = 0.1
            dPointX(2) = 0.1
            dPointX(3) = 0.0
            dPointX(4) = 0.0

            dPointY(0) = 0.0
            dPointY(1) = 0.0
            dPointY(2) = 0.1
            dPointY(3) = 0.1
            dPointY(4) = 0.0

            objAnnotAlignmentShapes = objSheet.AnnotAlignmentShapes

            ' for AddAnnotAlignmentShape and other properties specific to alignment shapes.
            objAnnotAlignmentShape = objAnnotAlignmentShapes.AddAnnotAlignmentShape(dPointX, dPointY)

        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub
End Class
See Also

AnnotAlignmentShapes Collection  | AnnotAlignmentShapes Members