Solid Edge FrameworkSupport Type Library
BringToFront Method
Description
Changes the display order of the referenced object by moving it in front of all other overlapping objects.
Syntax
Visual Basic
Public Sub BringToFront() 
Remarks
This command is useful when objects are hidden by other objects that are filled and have a higher priority display. The BringForward method can also be used.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objArcs2d As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc2d1 As SolidEdgeFrameworkSupport.Arc2d
    Dim objArc2d2 As SolidEdgeFrameworkSupport.Arc2d
    Dim objArc2d3 As SolidEdgeFrameworkSupport.Arc2d
    Dim lngOrder1 As Long
    Dim lngOrder2 As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create objArcs2d object
    Set objArcs2d = objSheet.Arcs2d
    ' Create 3 arcs
    Set objArc2d1 = objArcs2d.AddByStartAlongEnd(xStart:=0.233, yStart:=0.149, _
                                                 xAlong:=0.233, yAlong:=0.278, xEnd:=0.338, yEnd:=0.324)
    Set objArc2d2 = objArcs2d.AddByStartAlongEnd(xStart:=0.325, yStart:=0.16, _
                                                 xAlong:=0.269, yAlong:=0.293, xEnd:=0.158, yEnd:=0.34)
    Set objArc2d3 = objArcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
                                                  xStart:=0.15, yStart:=0#, xEnd:=0, yEnd:=0.15)
    'Get Zorder for objarc2d1 after bringing to front
    lngOrder1 = objArc2d1.ZOrder
    'Bring to front the first arc2d object
    Call objArc2d1.BringToFront
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objArcs2d = Nothing
    Set objArc2d1 = Nothing
    Set objArc2d2 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members